Wrapper struct that will contain the sequence of RAIL_BLE_TxChannelHoppingConfigEntry_t that represents the channel sequence to use during TX Channel Hopping.
Public Attributes#
Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.
This parameter must be set to the length of the buffer array.
The number of channels that is in the channel hopping sequence.
Pad bytes reserved for future use and currently ignored.
A pointer to the first element of an array of RAIL_BLE_TxChannelHoppingConfigEntry_t that represents the channels used during channel hopping.
Public Attribute Documentation#
buffer#
uint32_t* RAIL_BLE_TxChannelHoppingConfig_t::buffer
Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.
It need not be initialized and applications should never write data anywhere in this buffer.
bufferLength#
uint16_t RAIL_BLE_TxChannelHoppingConfig_t::bufferLength
This parameter must be set to the length of the buffer array.
This way, during configuration, the software can confirm it's writing within the range of the buffer. The configuration API will return an error if bufferLength is insufficient.
numberOfChannels#
uint8_t RAIL_BLE_TxChannelHoppingConfig_t::numberOfChannels
The number of channels that is in the channel hopping sequence.
reserved#
uint8_t RAIL_BLE_TxChannelHoppingConfig_t::reserved
Pad bytes reserved for future use and currently ignored.
entries#
RAIL_BLE_TxChannelHoppingConfigEntry_t* RAIL_BLE_TxChannelHoppingConfig_t::entries
A pointer to the first element of an array of RAIL_BLE_TxChannelHoppingConfigEntry_t that represents the channels used during channel hopping.
The length of this array must be numberOfChannels.