You are viewing documentation for version:
Data used for thermal protection. 
Public Attributes#
uint16_t
Store chip temperature for metrics. 
uint16_t
Minimum temperature recorded. 
uint16_t
Maximum temperature recorded. 
bool
Indicates if data should be reset. 
Public Attribute Documentation#
tempK#
uint16_t RAIL_ChipTempMetrics_t::tempK
Store chip temperature for metrics. 
minTempK#
uint16_t RAIL_ChipTempMetrics_t::minTempK
Minimum temperature recorded. 
maxTempK#
uint16_t RAIL_ChipTempMetrics_t::maxTempK
Maximum temperature recorded. 
resetPending#
bool RAIL_ChipTempMetrics_t::resetPending
Indicates if data should be reset. 
reservedChipTemp#
uint8_t RAIL_ChipTempMetrics_t::reservedChipTemp
Reserved for future use.