Chip-specific type that allows the user to specify direct mode parameters using RAIL_ConfigDirectMode().
Public Attributes#
Enable synchronous RX DOUT using DCLK vs.
Enable synchronous TX DIN using DCLK vs.
Only used with directRx.
Data output (DOUT) GPIO pin.
Only used in synchronous mode.
Data clock (DCLK) GPIO pin.
Only used with directTx.
Data frame (DIN) GPIO pin.
Data output (DOUT) location for pin/port.
Data clock (DCLK) location for pin/port.
Data frame (DIN) location for pin/port.
Public Attribute Documentation#
syncRx#
bool RAIL_DirectModeConfig_t::syncRx
Enable synchronous RX DOUT using DCLK vs.
asynchronous RX DOUT.
syncTx#
bool RAIL_DirectModeConfig_t::syncTx
Enable synchronous TX DIN using DCLK vs.
asynchronous TX DIN.
doutPort#
uint8_t RAIL_DirectModeConfig_t::doutPort
Only used with directRx.
Data output (DOUT) GPIO port
dclkPort#
uint8_t RAIL_DirectModeConfig_t::dclkPort
Only used in synchronous mode.
Data clock (DCLK) GPIO port. Only used in synchronous mode
dclkPin#
uint8_t RAIL_DirectModeConfig_t::dclkPin
Data clock (DCLK) GPIO pin.
Only used in synchronous mode