Contains elements of RAIL_BLE_AoxAntennaConfig_t struct.

Public Attributes#

uint8_t

The port which is used for AoX antenna switching.

uint8_t

The pin which is used for AoX antenna switching.

Public Attribute Documentation#

antPort#

uint8_t RAIL_BLE_AoxAntennaPortPins_t::antPort

The port which is used for AoX antenna switching.


Definition at line 724 of file protocol/ble/rail_ble.h

antPin#

uint8_t RAIL_BLE_AoxAntennaPortPins_t::antPin

The pin which is used for AoX antenna switching.


Definition at line 728 of file protocol/ble/rail_ble.h