Configuration information for FEM Voltage Detection plugin.

A structure of type RAIL_VdetConfig_t is passed to RAIL_ConfigVdet().

Public Attributes#

Mode for the VDET.

Resolution to use for the capture.

uint32_t

Delay in us for the capture from Tx Start in RAIL_VDET_MODE_AUTOMATIC.

Public Attribute Documentation#

mode#

RAIL_Vdet_Mode_t RAIL_VdetConfig_t::mode

Mode for the VDET.


Definition at line 5740 of file common/rail_types.h

resolution#

RAIL_Vdet_Resolution_t RAIL_VdetConfig_t::resolution

Resolution to use for the capture.


Definition at line 5742 of file common/rail_types.h

delayUs#

uint32_t RAIL_VdetConfig_t::delayUs

Delay in us for the capture from Tx Start in RAIL_VDET_MODE_AUTOMATIC.

Minimum 5us, maximum 100ms


Definition at line 5744 of file common/rail_types.h