A configuration for antenna selection.
Public Attributes#
Antenna 0 Pin Enable.
Antenna 1 Pin Enable.
A RAIL_AntennaSel_t value specifying the internal default RF path.
Antenna 0 output GPIO port.
Antenna 0 output GPIO pin.
Antenna 1 output GPIO port.
Antenna 1 output GPIO pin.
Public Attribute Documentation#
defaultPath#
uint8_t RAIL_AntennaConfig_t::defaultPath
A RAIL_AntennaSel_t value specifying the internal default RF path.
It is ignored on EFR32 parts that have only one RF path bonded out and on EFR32xG28 dual-band OPNs where the appropriate RF path is automatically set by RAIL to 0 for 2.4 GHz band and 1 for Sub-GHz band PHYs. On EFR32xG23 and EFR32xG28 single-band OPNs where both RF paths are bonded out this can be set to RAIL_ANTENNA_AUTO to effect internal RF path diversity on PHYs supporting diversity. This avoids the need for an external RF switch and the associated GPIO(s) needed to control its antenna selection.