A structure for BLE radio state parameters.
DeprecatedRAIL 2.x synonym of sl_rail_ble_state_t.
Public Attributes#
The value used to initialize the CRC algorithm.
The access address used for the connection.
The logical channel used.
Indicates whether the whitening engine should be off (generally used for testing only).
Reserved for future use; specify 0.
Public Attribute Documentation#
crcInit#
uint32_t RAIL_BLE_State_t::crcInit
The value used to initialize the CRC algorithm.
DeprecatedRAIL 2.x synonym of sl_rail_ble_state_t::crc_init.
accessAddress#
uint32_t RAIL_BLE_State_t::accessAddress
The access address used for the connection.
It is transmitted or received least-significant bit first.
DeprecatedRAIL 2.x synonym of sl_rail_ble_state_t::access_address.
channel#
uint16_t RAIL_BLE_State_t::channel
The logical channel used.
DeprecatedRAIL 2.x synonym of sl_rail_ble_state_t::logical_channel.
disableWhitening#
bool RAIL_BLE_State_t::disableWhitening
Indicates whether the whitening engine should be off (generally used for testing only).
DeprecatedRAIL 2.x synonym of sl_rail_ble_state_t::disable_whitening.
whiteInit#
uint16_t RAIL_BLE_State_t::whiteInit
Reserved for future use; specify 0.
DeprecatedRAIL 2.x synonym of sl_rail_ble_state_t::white_init.