Angle of Arrival/Departure#
These APIs are to a stack implementing BLE's angle of arrival and angle of departure functionality.
They are designed for use by the Silicon Labs BLE stack only at this time and may cause problems if accessed directly.
Modules#
sl_rail_ble_aox_antenna_port_pins_t
sl_rail_ble_aox_antenna_config_t
Enumerations#
Angle of Arrival/Departure options bit fields.
Angle of Arrival/Departure options bit fields.
Functions#
Lock/unlock the CTE buffer from the application's perspective.
Determine whether the CTE buffer is currently locked or not.
Get the offset into CTE sample of CTE data.
Get the effective sample rate used by the ADC to capture the CTE samples.
Configure Angle of Arrival/Departure (AoX) functionality.
Perform one time initialization of AoX registers.
Perform initialization of AoX antenna GPIO pins.
Lock/unlock the CTE buffer from the application's perspective.
Determine whether the CTE buffer is currently locked or not.
Get the offset into CTE sample of CTE data.
Get the effective sample rate used by the ADC to capture the CTE samples.
Configure Angle of Arrival/Departure (AoX) functionality.
Perform one time initialization of AoX registers.
Perform initialization of AoX antenna GPIO pins.
Macros#
The maximum number of GPIO pins used for AoX Antenna switching.
DeprecatedObsolete AOX option.
DeprecatedObsolete AOX option.
DeprecatedObsolete AOX option.
DeprecatedUse SL_RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK_SHIFT instead.
Disable the AoX feature.
Sets one of the two AoX sampling/switching modes: 1 us or 2 us window.
Enables connectionless AoX Rx packets.
Enables connection based AoX Rx packets.
Disables CTE buffer lock.
Enables connection based or connectionless AoX Rx packets.
The maximum number of GPIO pins used for AoX Antenna switching.
Disable the AoX feature.
Sets one of the two AoX sampling/switching modes: 1 us or 2 us window.
Enables connectionless AoX Rx packets.
Enables connection based AoX Rx packets.
Disables CTE buffer lock.
Enables connection based or connectionless AoX Rx packets.
Enumeration Documentation#
RAIL_BLE_AoxOptions_t#
RAIL_BLE_AoxOptions_t
Angle of Arrival/Departure options bit fields.
DeprecatedRAIL 2.x synonym of sl_rail_ble_aox_options_t.
| Enumerator | |
|---|---|
| RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE bit. |
| RAIL_BLE_AOX_OPTIONS_CONNLESS_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_CONNLESS bit. |
| RAIL_BLE_AOX_OPTIONS_CONN_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_CONN bit. |
| RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK bit. |
sl_rail_ble_aox_options_t#
sl_rail_ble_aox_options_t
Angle of Arrival/Departure options bit fields.
| Enumerator | |
|---|---|
| SL_RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE_SHIFT | Shift position of SL_RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE bit. |
| SL_RAIL_BLE_AOX_OPTIONS_CONNLESS_SHIFT | Shift position of SL_RAIL_BLE_AOX_OPTIONS_CONNLESS bit. |
| SL_RAIL_BLE_AOX_OPTIONS_CONN_SHIFT | Shift position of SL_RAIL_BLE_AOX_OPTIONS_CONN bit. |
| SL_RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK_SHIFT | Shift position of SL_RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK bit. |
Function Documentation#
RAIL_BLE_LockCteBuffer#
bool RAIL_BLE_LockCteBuffer (RAIL_Handle_t railHandle, bool lock)
Lock/unlock the CTE buffer from the application's perspective.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | lock | Lock the CTE buffer if true and unlock it if false. |
The radio will write to the buffer only if the bit is NOT set at the beginning of the sampling period. The radio will set the bit once the sampling period starts to indicate that some CTE data has been collected, which will not be overwritten during the next sampling period, unless the buffer is unlocked by the application.
Returns
true if the CTE buffer is locked after the call, otherwise false.
DeprecatedRAIL 2.x synonym of sl_rail_ble_lock_cte_buffer().
RAIL_BLE_CteBufferIsLocked#
bool RAIL_BLE_CteBufferIsLocked (RAIL_Handle_t railHandle)
Determine whether the CTE buffer is currently locked or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle for RAIL instance. |
Returns
true if CTE buffer is locked and false otherwise.
DeprecatedRAIL 2.x synonym of sl_rail_ble_cte_buffer_is_locked().
RAIL_BLE_GetCteSampleOffset#
uint8_t RAIL_BLE_GetCteSampleOffset (RAIL_Handle_t railHandle)
Get the offset into CTE sample of CTE data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle for RAIL instance. |
Returns
The offset of CTE data in a CTE sample in bytes. On unsupported platforms this returns 0.
DeprecatedRAIL 2.x synonym of sl_rail_ble_get_cte_sample_offset().
RAIL_BLE_GetCteSampleRate#
uint32_t RAIL_BLE_GetCteSampleRate (RAIL_Handle_t railHandle)
Get the effective sample rate used by the ADC to capture the CTE samples.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle for RAIL instance. |
Returns
The actual sample rate used to capture the CTE in samples per second. On unsupported platforms this returns 0.
DeprecatedRAIL 2.x synonym of sl_rail_ble_get_cte_sample_rate().
RAIL_BLE_ConfigAox#
RAIL_Status_t RAIL_BLE_ConfigAox (RAIL_Handle_t railHandle, const RAIL_BLE_AoxConfig_t * aoxConfig)
Configure Angle of Arrival/Departure (AoX) functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_BLE_AoxConfig_t * | [in] | aoxConfig | Configuration options for AoX |
Returns
Status code indicating success of the function call.
AoX is a method of radio localization which infers angle of arrival/departure of the signal based on different phases of the raw I/Q signal from different antennas by controlling external RF switch during the continuous tone extension (CTE). Connection based AoX packets are different than normal BLE packets in that they have 3 header bytes instead of 2 and they have CTE appended after the payload's CRC. 3rd byte or CTE info contains CTE length. Connectionless AoX packets have 2 header bytes and CTE info is part of the payload.
Note
Calling RAIL_GetRadioEntropy() during AoX reception may break packet reception.
DeprecatedRAIL 2.x synonym of sl_rail_ble_config_aox().
RAIL_BLE_InitCte#
RAIL_Status_t RAIL_BLE_InitCte (RAIL_Handle_t railHandle)
Perform one time initialization of AoX registers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
This function must be called before RAIL_BLE_ConfigAox() and before configuring the BLE PHY.
Returns
Status code indicating success of the function call.
DeprecatedRAIL 2.x synonym of sl_rail_ble_init_cte().
RAIL_BLE_ConfigAoxAntenna#
RAIL_Status_t RAIL_BLE_ConfigAoxAntenna (RAIL_Handle_t railHandle, const RAIL_BLE_AoxAntennaConfig_t * antennaConfig)
Perform initialization of AoX antenna GPIO pins.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_BLE_AoxAntennaConfig_t * | [in] | antennaConfig | A pointer to the antenna configuration structure to hold the set of GPIO ports and pins for AoX antenna switching. |
This function must be called before calls to RAIL_BLE_InitCte() and RAIL_BLE_ConfigAox(), and before configuring the BLE PHY, else a RAIL_STATUS_INVALID_CALL is returned.
If user configures more pins in RAIL_BLE_AoxAntennaConfig_t::antCount than allowed by RAIL_BLE_AOX_ANTENNA_PIN_COUNT, then the API returns RAIL_STATUS_INVALID_PARAMETER.
If user configures lesser than or equal to number of pins allowed by RAIL_BLE_AOX_ANTENNA_PIN_COUNT, then the requested number of pins are configured and RAIL_STATUS_NO_ERROR is returned.
If AoX antenna switching is inactive, non-AoX transmits and receives will occur on the first antenna specified by the antenna pattern or on the default antenna if no antenna pattern is provided.
Note
This function must only be called while channel sounding is disabled. If channel sounding has been enabled RAIL_STATUS_INVALID_STATE will be returned.
Returns
Status code indicating success of the function call.
Note
Use the compile time symbol RAIL_BLE_SUPPORTS_ANTENNA_SWITCHING or the runtime call RAIL_BLE_SupportsAntennaSwitching() to check whether the platform supports this feature.
Warnings
As this function relies on GPIO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if GPIO is configured as secure peripheral and it will return RAIL_STATUS_INVALID_CALL.
DeprecatedRAIL 2.x synonym of sl_rail_ble_config_aox_antenna().
sl_rail_ble_lock_cte_buffer#
bool sl_rail_ble_lock_cte_buffer (sl_rail_handle_t rail_handle, bool lock)
Lock/unlock the CTE buffer from the application's perspective.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| bool | [in] | lock | Lock the CTE buffer if true and unlock it if false. |
The radio will write to the buffer only if the bit is NOT set at the beginning of the sampling period. The radio will set the bit once the sampling period starts to indicate that some CTE data has been collected, which will not be overwritten during the next sampling period, unless the buffer is unlocked by the application.
Returns
true if the CTE buffer is locked after the call, otherwise false.
sl_rail_ble_cte_buffer_is_locked#
bool sl_rail_ble_cte_buffer_is_locked (sl_rail_handle_t rail_handle)
Determine whether the CTE buffer is currently locked or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
true if CTE buffer is locked and false otherwise.
sl_rail_ble_get_cte_sample_offset#
uint8_t sl_rail_ble_get_cte_sample_offset (sl_rail_handle_t rail_handle)
Get the offset into CTE sample of CTE data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
The offset of CTE data in a CTE sample in bytes. On unsupported platforms this returns 0.
sl_rail_ble_get_cte_sample_rate#
uint32_t sl_rail_ble_get_cte_sample_rate (sl_rail_handle_t rail_handle)
Get the effective sample rate used by the ADC to capture the CTE samples.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
The actual sample rate used to capture the CTE in samples per second. On unsupported platforms this returns 0.
sl_rail_ble_config_aox#
sl_rail_status_t sl_rail_ble_config_aox (sl_rail_handle_t rail_handle, const sl_rail_ble_aox_config_t * p_aox_config)
Configure Angle of Arrival/Departure (AoX) functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| const sl_rail_ble_aox_config_t * | [in] | p_aox_config | A pointer to AoX configuration settings. |
Returns
Status code indicating success of the function call.
AoX is a method of radio localization which infers angle of arrival/departure of the signal based on different phases of the raw I/Q signal from different antennas by controlling external RF switch during the continuous tone extension (CTE). Connection based AoX packets are different than normal BLE packets in that they have 3 header bytes instead of 2 and they have CTE appended after the payload's CRC. 3rd byte or CTE info contains CTE length. Connectionless AoX packets have 2 header bytes and CTE info is part of the payload.
Note
Calling sl_rail_get_radio_entropy() during AoX reception may break packet reception.
sl_rail_ble_init_cte#
sl_rail_status_t sl_rail_ble_init_cte (sl_rail_handle_t rail_handle)
Perform one time initialization of AoX registers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
This function must be called before sl_rail_ble_config_aox() and before configuring the BLE PHY.
Returns
Status code indicating success of the function call.
sl_rail_ble_config_aox_antenna#
sl_rail_status_t sl_rail_ble_config_aox_antenna (sl_rail_handle_t rail_handle, const sl_rail_ble_aox_antenna_config_t * p_antenna_config)
Perform initialization of AoX antenna GPIO pins.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| const sl_rail_ble_aox_antenna_config_t * | [in] | p_antenna_config | A pointer to the antenna configuration structure to hold the set of GPIO ports and pins for AoX antenna switching. |
This function must be called before calls to sl_rail_ble_init_cte() and sl_rail_ble_config_aox(), and before configuring the BLE PHY, else a SL_RAIL_STATUS_INVALID_CALL is returned.
If user configures more pins in sl_rail_ble_aox_antenna_config_t::antenna_count than allowed by SL_RAIL_BLE_AOX_ANTENNA_PIN_COUNT, then the API returns SL_RAIL_STATUS_INVALID_PARAMETER.
If user configures lesser than or equal to number of pins allowed by SL_RAIL_BLE_AOX_ANTENNA_PIN_COUNT, then the requested number of pins are configured and SL_RAIL_STATUS_NO_ERROR is returned.
If AoX antenna switching is inactive, non-AoX transmits and receives will occur on the first antenna specified by the antenna pattern or on the default antenna if no antenna pattern is provided.
Note
This function must only be called while channel sounding is disabled. If channel sounding has been enabled SL_RAIL_STATUS_INVALID_STATE will be returned.
Returns
Status code indicating success of the function call.
Note
Use the compile time symbol SL_RAIL_BLE_SUPPORTS_ANTENNA_SWITCHING or the runtime call sl_rail_ble_supports_antenna_switching() to check whether the platform supports this feature.
Warnings
As this function relies on GPIO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if GPIO is configured as secure peripheral and it will return SL_RAIL_STATUS_INVALID_CALL.