Contains elements of RAIL_BLE_AoxAntennaConfig_t struct.

DeprecatedRAIL 2.x synonym of sl_rail_ble_aox_antenna_port_pins_t.

Public Attributes#

uint8_t

The port which is used for AoX antenna switching.

uint8_t

The pin which is used for AoX antenna switching.

Public Attribute Documentation#

antPort#

uint8_t RAIL_BLE_AoxAntennaPortPins_t::antPort

The port which is used for AoX antenna switching.

DeprecatedRAIL 2.x synonym of sl_rail_ble_aox_antenna_port_pins_t::antenna_port.


antPin#

uint8_t RAIL_BLE_AoxAntennaPortPins_t::antPin

The pin which is used for AoX antenna switching.

DeprecatedRAIL 2.x synonym of sl_rail_ble_aox_antenna_port_pins_t::antenna_pin.