Allows the user to specify direct mode parameters using RAIL_ConfigDirectMode().
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t.
Public Attributes#
Enable synchronous RX DOUT using DCLK vs.
Enable synchronous TX DIN using DCLK vs.
RX Data output (DOUT) GPIO port.
RX Data output (DOUT) GPIO pin.
Data clock (DCLK) GPIO port.
Data clock (DCLK) GPIO pin.
TX Data input (DIN) GPIO port.
TX Data input (DIN) GPIO pin.
Public Attribute Documentation#
syncRx#
bool RAIL_DirectModeConfig_t::syncRx
Enable synchronous RX DOUT using DCLK vs.
asynchronous RX DOUT.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::sync_rx.
syncTx#
bool RAIL_DirectModeConfig_t::syncTx
Enable synchronous TX DIN using DCLK vs.
asynchronous TX DIN.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::sync_tx.
doutPort#
uint8_t RAIL_DirectModeConfig_t::doutPort
RX Data output (DOUT) GPIO port.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::dout_port.
doutPin#
uint8_t RAIL_DirectModeConfig_t::doutPin
RX Data output (DOUT) GPIO pin.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::dout_pin.
dclkPort#
uint8_t RAIL_DirectModeConfig_t::dclkPort
Data clock (DCLK) GPIO port.
Only used in synchronous mode.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::dclk_port.
dclkPin#
uint8_t RAIL_DirectModeConfig_t::dclkPin
Data clock (DCLK) GPIO pin.
Only used in synchronous mode.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::dclk_pin.
dinPort#
uint8_t RAIL_DirectModeConfig_t::dinPort
TX Data input (DIN) GPIO port.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::din_port.
dinPin#
uint8_t RAIL_DirectModeConfig_t::dinPin
TX Data input (DIN) GPIO pin.
DeprecatedRAIL 2.x synonym of sl_rail_direct_mode_config_t::din_pin.
doutLoc#
uint8_t RAIL_DirectModeConfig_t::doutLoc
DeprecatedNo longer used (ignored); see sl_rail_direct_mode_config_t::reserved_0.
dclkLoc#
uint8_t RAIL_DirectModeConfig_t::dclkLoc
DeprecatedNo longer used (ignored); see sl_rail_direct_mode_config_t::reserved_1.
dinLoc#
uint8_t RAIL_DirectModeConfig_t::dinLoc
DeprecatedNo longer used (ignored); see sl_rail_direct_mode_config_t::reserved_2.