A structure containing values used to initialize the power amplifiers.
Public Attributes#
TX power mode.
uint16_t
Power amplifier supply voltage in mV, generally: DCDC supply ~ 1800 mV (1.8 V) Battery supply ~ 3300 mV (3.3 V)
uint16_t
The amount of time to spend ramping for TX in microseconds.
Public Attribute Documentation#
voltage_mv#
uint16_t sl_rail_tx_power_config_t::voltage_mv
Power amplifier supply voltage in mV, generally: DCDC supply ~ 1800 mV (1.8 V) Battery supply ~ 3300 mV (3.3 V)
ramp_time_us#
uint16_t sl_rail_tx_power_config_t::ramp_time_us
The amount of time to spend ramping for TX in microseconds.