Import and Export #

Simplicity Studio® 5 (SSv5) File > Import and File > Export options allow you to import a project from Keil® µVision4®, IAR Embedded Workbench, or the 8-bit Silicon Labs IDE into Simplicity IDE, and to export a project in a variety of formats.

Import #

Select File > Import , and locate the folder with the project to be imported.

Select the project and click Next . If anything about the project is unresolved you can resolve it.

Click Next . Name the project and click Finish .

Export #

Select File > Export , and select the file(s) to be exported.

The default export format is an .sls file, which can easily be re-imported into SSv5. However, other options are available. Click More export options... and select a wizard.