Migrate from SSv4 #
The process to migrate a project from Simplicity Studio® 4 (SSv4) to Simplicity Studio 5 (SSv5) depends on the type of project.
If you are migrating a Z-Wave, Bootloader, EFM32, or EFM8 project , use the Migrate Project tool. If you are migrating a Bluetooth, Proprietary Flex, or Zigbee project , follow the instructions in the specified documents.
Z-Wave, Bootloader, EFM32, and EFM8 Projects #
Click the Tools toolbar button to open the Tools dialog. Select Migrate Projects and click OK . Select the project to be migrated and click Next .
Verify the information displayed and click Next .
Decide if you want to copy the project (recommended) and click Finish .
The project is migrated from SSv4 to SSv5.
Zigbee, Flex, and Bluetooth Projects #
These projects cannot be migrated using the tool. If you try, the tool will point you to the documentation for the migration process.
The documents are: