GENERAL_API


General API messages available in both split and full MAC.

Modules

General_Configuration
General configuration commands.
Secure_Link
APIs for Secure link configuration and usage.
Prevent_Firmware_Rollback
APIs for preventing Rollback of unsafe firmware images.
PTA
APIs to manage dynamic aspects of Packet Traffic Arbitration (PTA).
ERROR_IDS

Data Structures

union sl_wfx_general_commands_ids_t
General command message IDs.
struct sl_wfx_set_cca_config_req_body_t
Request sent by host to set the Clear Channel Assessment configuration Set the CCA mode and the defer threshold.
struct sl_wfx_set_cca_config_cnf_body_t
Confirmation sent by Wlan firmware after a SL_WFX_SET_CCA_CONFIG_REQ_ID request.

Enumerations

enum sl_wfx_generic_requests_ids_t {
SL_WFX_CONFIGURATION_REQ_ID = 0x09,
SL_WFX_CONTROL_GPIO_REQ_ID = 0x26,
SL_WFX_SET_SECURELINK_MAC_KEY_REQ_ID = 0x27,
SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_REQ_ID = 0x28,
SL_WFX_SECURELINK_CONFIGURE_REQ_ID = 0x29,
SL_WFX_PREVENT_ROLLBACK_REQ_ID = 0x2a,
SL_WFX_PTA_SETTINGS_REQ_ID = 0x2b,
SL_WFX_PTA_PRIORITY_REQ_ID = 0x2c,
SL_WFX_PTA_STATE_REQ_ID = 0x2d,
SL_WFX_SET_CCA_CONFIG_REQ_ID = 0x2e,
SL_WFX_SHUT_DOWN_REQ_ID = 0x32
}
General request message IDs.
enum sl_wfx_general_confirmations_ids_t {
SL_WFX_CONFIGURATION_CNF_ID = 0x09,
SL_WFX_CONTROL_GPIO_CNF_ID = 0x26,
SL_WFX_SET_SECURELINK_MAC_KEY_CNF_ID = 0x27,
SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_CNF_ID = 0x28,
SL_WFX_SECURELINK_CONFIGURE_CNF_ID = 0x29,
SL_WFX_PREVENT_ROLLBACK_CNF_ID = 0x2a,
SL_WFX_PTA_SETTINGS_CNF_ID = 0x2b,
SL_WFX_PTA_PRIORITY_CNF_ID = 0x2c,
SL_WFX_PTA_STATE_CNF_ID = 0x2d,
SL_WFX_SET_CCA_CONFIG_CNF_ID = 0x2e
}
General confirmation message IDs.
enum sl_wfx_general_indications_ids_t {
SL_WFX_EXCEPTION_IND_ID = 0xe0,
SL_WFX_STARTUP_IND_ID = 0xe1,
SL_WFX_WAKEUP_IND_ID = 0xe2,
SL_WFX_GENERIC_IND_ID = 0xe3,
SL_WFX_ERROR_IND_ID = 0xe4,
SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_IND_ID = 0xe5
}
General indications message IDs.
enum sl_wfx_status_t {
SL_WFX_STATUS_SUCCESS = 0x0,
SL_WFX_STATUS_FAILURE = 0x1,
SL_WFX_INVALID_PARAMETER = 0x2,
SL_WFX_STATUS_GPIO_WARNING = 0x3,
SL_WFX_ERROR_UNSUPPORTED_MSG_ID = 0x4,
SL_WFX_MAC_KEY_STATUS_SUCCESS = 0x5A,
SL_WFX_MAC_KEY_STATUS_FAILED_KEY_ALREADY_BURNED = 0x6B,
SL_WFX_MAC_KEY_STATUS_FAILED_RAM_MODE_NOT_ALLOWED = 0x7C,
SL_WFX_MAC_KEY_STATUS_FAILED_UNKNOWN_MODE = 0x8D,
SL_WFX_PUB_KEY_EXCHANGE_STATUS_SUCCESS = 0x9E,
SL_WFX_PUB_KEY_EXCHANGE_STATUS_FAILED = 0xAF,
SL_WFX_PREVENT_ROLLBACK_CNF_SUCCESS = 0x1234,
SL_WFX_PREVENT_ROLLBACK_CNF_WRONG_MAGIC_WORD = 0x1256
}
General confirmation possible values for returned 'status' field WLAN All general confirmation messages have a field 'status' just after the message header.
enum sl_wfx_cc_thr_mode_t {
SL_WFX_CCA_THR_MODE_RELATIVE = 0x0,
SL_WFX_CCA_THR_MODE_ABSOLUTE = 0x1
}
CCA Mode definition.

Detailed Description


General API messages available in both split and full MAC.

Mainly used to boot and configure the part.
But some message are also used to report errors or information.

  • general requests are sl_wfx_generic_requests_ids_t
  • general indications are sl_wfx_general_indications_ids_t


Data Structure Documentation

◆ sl_wfx_general_commands_ids_t

union sl_wfx_general_commands_ids_t

General command message IDs.

All general API message IDs.

Definition at line 218 of file sl_wfx_general_api.h .

Data Fields
sl_wfx_general_confirmations_ids_t confirmation Confirmation of a request from the WLAN device to the host.
sl_wfx_general_indications_ids_t indication Indication from the WLAN device to the host.
sl_wfx_generic_requests_ids_t request Request from the host to the WLAN device.

◆ sl_wfx_set_cca_config_req_body_t

struct sl_wfx_set_cca_config_req_body_t

Request sent by host to set the Clear Channel Assessment configuration Set the CCA mode and the defer threshold.

Definition at line 982 of file sl_wfx_general_api.h .

Data Fields
uint8_t cca_thr_mode CCA threshold mode. See enum sl_wfx_cc_thr_mode_t .
uint8_t reserved[3] reserved for future use, set to 0

◆ sl_wfx_set_cca_config_cnf_body_t

struct sl_wfx_set_cca_config_cnf_body_t

Confirmation sent by Wlan firmware after a SL_WFX_SET_CCA_CONFIG_REQ_ID request.

Definition at line 995 of file sl_wfx_general_api.h .

Data Fields
uint32_t status Confirmation status, see enum sl_wfx_status_t .

Enumeration Type Documentation

◆ sl_wfx_cc_thr_mode_t

CCA Mode definition.

Enumerator
SL_WFX_CCA_THR_MODE_RELATIVE

Use CCA defer threshold relative to channel noise.

SL_WFX_CCA_THR_MODE_ABSOLUTE

Use absolute CCA defer threshold.

Definition at line 973 of file sl_wfx_general_api.h .

◆ sl_wfx_general_confirmations_ids_t

General confirmation message IDs.

API general confirmation message IDs returned by requests described in sl_wfx_general_requests_ids. These are messages from the WLAN towards the host.

Enumerator
SL_WFX_CONFIGURATION_CNF_ID

CONFIGURATION confirmation Id returns body sl_wfx_configuration_cnf_body_t

SL_WFX_CONTROL_GPIO_CNF_ID

CONTROL_GPIO confirmation Id returns body sl_wfx_control_gpio_cnf_body_t

SL_WFX_SET_SECURELINK_MAC_KEY_CNF_ID

SET_SECURELINK_MAC_KEY confirmation Id returns body sl_wfx_set_securelink_mac_key_cnf_body_t

SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_CNF_ID

SECURELINK_EXCHANGE_PUB_KEYS confirmation Id returns body sl_wfx_securelink_exchange_pub_keys_cnf_body_t

SL_WFX_SECURELINK_CONFIGURE_CNF_ID

SECURELINK_CONFIGURE confirmation Id returns body sl_wfx_securelink_configure_cnf_body_t

SL_WFX_PREVENT_ROLLBACK_CNF_ID

PREVENT_ROLLBACK confirmation Id use body sl_wfx_prevent_rollback_cnf_body_t

SL_WFX_PTA_SETTINGS_CNF_ID

PTA_SETTINGS confirmation Id returns sl_wfx_pta_settings_cnf_body_t

SL_WFX_PTA_PRIORITY_CNF_ID

PTA_PRIORITY confirmation Id returns sl_wfx_pta_priority_cnf_body_t

SL_WFX_PTA_STATE_CNF_ID

PTA_STATE confirmation Id returns sl_wfx_pta_state_cnf_body_t

SL_WFX_SET_CCA_CONFIG_CNF_ID

SET_CCA_CONFIG confirmation Id returns body sl_wfx_set_cca_config_cnf_body_t

Definition at line 185 of file sl_wfx_general_api.h .

◆ sl_wfx_general_indications_ids_t

General indications message IDs.

API general indication message IDs available in both split and full MAC. These are messages from the WLAN towards the host.

Enumerator
SL_WFX_EXCEPTION_IND_ID

EXCEPTION indication Id content is sl_wfx_exception_ind_body_t

SL_WFX_STARTUP_IND_ID

STARTUP indication Id content is sl_wfx_startup_ind_body_t

SL_WFX_WAKEUP_IND_ID

WAKE UP indication Id has no content

SL_WFX_GENERIC_IND_ID

GENERIC indication Id content is sl_wfx_generic_ind_body_t

SL_WFX_ERROR_IND_ID

ERROR indication Id content is sl_wfx_error_ind_body_t

SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_IND_ID

SECURELINK_EXCHANGE_PUB_KEYS indication Id content is sl_wfx_securelink_exchange_pub_keys_ind_body_t

Definition at line 204 of file sl_wfx_general_api.h .

◆ sl_wfx_generic_requests_ids_t

General request message IDs.

API general request message IDs available in both split and full MAC. These are messages from the host towards the WLAN.

Enumerator
SL_WFX_CONFIGURATION_REQ_ID

CONFIGURATION request Id use body sl_wfx_configuration_req_body_t and returns sl_wfx_configuration_cnf_body_t

SL_WFX_CONTROL_GPIO_REQ_ID

CONTROL_GPIO request Id use body sl_wfx_control_gpio_req_body_t and returns sl_wfx_control_gpio_cnf_body_t

SL_WFX_SET_SECURELINK_MAC_KEY_REQ_ID

SET_SECURELINK_MAC_KEY request Id use body sl_wfx_set_securelink_mac_key_req_body_t and returns sl_wfx_set_securelink_mac_key_cnf_body_t

SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_REQ_ID

SECURELINK_EXCHANGE_PUB_KEYS request Id use body sl_wfx_securelink_exchange_pub_keys_req_body_t and returns sl_wfx_securelink_exchange_pub_keys_cnf_body_t

SL_WFX_SECURELINK_CONFIGURE_REQ_ID

SECURELINK_CONFIGURE request Id use body sl_wfx_securelink_configure_req_body_t and returns sl_wfx_securelink_exchange_pub_keys_cnf_body_t

SL_WFX_PREVENT_ROLLBACK_REQ_ID

PREVENT_ROLLBACK request Id use body sl_wfx_prevent_rollback_req_body_t and returns sl_wfx_prevent_rollback_cnf_body_t

SL_WFX_PTA_SETTINGS_REQ_ID

PTA_SETTINGS request Id use body sl_wfx_pta_settings_req_body_t and returns sl_wfx_pta_settings_cnf_body_t

SL_WFX_PTA_PRIORITY_REQ_ID

PTA_PRIORITY request Id use body sl_wfx_pta_priority_req_body_t and returns sl_wfx_pta_priority_cnf_body_t

SL_WFX_PTA_STATE_REQ_ID

PTA_STATE request Id use body sl_wfx_pta_state_req_body_t and returns sl_wfx_pta_state_cnf_body_t

SL_WFX_SET_CCA_CONFIG_REQ_ID

SET_CCA_CONFIG request Id uses body sl_wfx_set_cca_config_req_body_t and returns sl_wfx_set_cca_config_cnf_body_t

SL_WFX_SHUT_DOWN_REQ_ID

SHUT_DOWN request Id use body sl_wfx_shut_down_req_t and never returns

Definition at line 165 of file sl_wfx_general_api.h .

◆ sl_wfx_status_t

General confirmation possible values for returned 'status' field WLAN All general confirmation messages have a field 'status' just after the message header.


A value of zero indicates the request is completed successfully.

Enumerator
SL_WFX_STATUS_SUCCESS

The firmware has successfully completed the request.

SL_WFX_STATUS_FAILURE

This is a generic failure code : other error codes do not apply.

SL_WFX_INVALID_PARAMETER

The request contains one or more invalid parameters.

SL_WFX_STATUS_GPIO_WARNING

Warning : the GPIO CMD is successful but the read value is not as expected (likely a drive conflict on the line)

SL_WFX_ERROR_UNSUPPORTED_MSG_ID

Unknown request ID or wrong interface ID used.

SL_WFX_MAC_KEY_STATUS_SUCCESS

Key has been correctly written.

SL_WFX_MAC_KEY_STATUS_FAILED_KEY_ALREADY_BURNED

Key already exists in OTP.

SL_WFX_MAC_KEY_STATUS_FAILED_RAM_MODE_NOT_ALLOWED

RAM mode is not allowed.

SL_WFX_MAC_KEY_STATUS_FAILED_UNKNOWN_MODE

Unknown mode (should be RAM or OTP)

SL_WFX_PUB_KEY_EXCHANGE_STATUS_SUCCESS

Host Public Key authenticated.

SL_WFX_PUB_KEY_EXCHANGE_STATUS_FAILED

Host Public Key authentication failed.

SL_WFX_PREVENT_ROLLBACK_CNF_SUCCESS

OTP rollback value has been successfully updated.

SL_WFX_PREVENT_ROLLBACK_CNF_WRONG_MAGIC_WORD

Wrong magic word detected.

Definition at line 233 of file sl_wfx_general_api.h .