sl_wfx_nonce_t Struct Reference

Structure to maintain secure link counters.

Data Fields

uint32_t hp_packet_count
High priority packet counter.
uint32_t rx_packet_count
Received packet counter.
uint32_t tx_packet_count
Sent packet counter.

Structure to maintain secure link counters.

Definition at line 368 of file sl_wfx_constants.h .

Field Documentation

◆ hp_packet_count

uint32_t sl_wfx_nonce_t::hp_packet_count

High priority packet counter.

Definition at line 369 of file sl_wfx_constants.h .

◆ rx_packet_count

uint32_t sl_wfx_nonce_t::rx_packet_count

Received packet counter.

Definition at line 370 of file sl_wfx_constants.h .

◆ tx_packet_count

uint32_t sl_wfx_nonce_t::tx_packet_count

Sent packet counter.

Definition at line 371 of file sl_wfx_constants.h .


The documentation for this struct was generated from the following file:
  • sl_wfx_constants.h