GENERAL_DRIVER_API
Functions | |
sl_status_t | sl_wfx_secure_link_set_mac_key (const uint8_t *sl_mac_key, sl_wfx_securelink_mac_key_dest_t destination) |
SecureLink Set MAC Key. | |
sl_status_t | sl_wfx_secure_link_exchange_keys (const uint8_t *sl_mac_key, uint8_t *sl_host_pub_key) |
Exchange SecureLink public keys. | |
sl_status_t | sl_wfx_secure_link_renegotiate_session_key (void) |
Renegotiate session key request. | |
sl_status_t | sl_wfx_secure_link_configure (const uint8_t *encryption_bitmap, uint8_t disable_session_key_protection) |
Modify SecureLink configuration. | |
sl_status_t | sl_wfx_send_configuration (const char *pds_data, uint32_t pds_data_length) |
Function to send PDS chunks. | |
sl_status_t | sl_wfx_control_gpio (uint8_t gpio_label, uint8_t gpio_mode, uint32_t *value) |
Send a request to read or write a GPIO. | |
sl_status_t | sl_wfx_pta_settings (uint8_t pta_mode, uint8_t request_signal_active_level, uint8_t priority_signal_active_level, uint8_t freq_signal_active_level, uint8_t grant_signal_active_level, uint8_t coex_type, uint8_t default_grant_state, uint8_t simultaneous_rx_access, uint8_t priority_sampling_time, uint8_t tx_rx_sampling_time, uint8_t freq_sampling_time, uint8_t grant_valid_time, uint8_t fem_control_time, uint8_t first_slot_time, uint16_t periodic_tx_rx_sampling_time, uint16_t coex_quota, uint16_t wlan_quota) |
Send a request to set the PTA mode, the active levels on signals, the Coex type, to define the timings, quotas, combined mode and default grant state. | |
sl_status_t | sl_wfx_pta_priority (uint32_t priority) |
Send a request to define the level of priority used to arbitrate concurrent Coex and Wlan requests. | |
sl_status_t | sl_wfx_pta_state (uint32_t pta_state) |
Send a request to start or stop the PTA. | |
sl_status_t | sl_wfx_set_cca_config (uint8_t cca_thr_mode) |
Send a request to configure the CCA mode. | |
sl_status_t | sl_wfx_prevent_rollback (uint32_t magic_word) |
Prevent Rollback request. | |
sl_status_t | sl_wfx_shutdown (void) |
Shutdown the Wi-Fi chip. |
Function Documentation
◆ sl_wfx_control_gpio()
sl_status_t sl_wfx_control_gpio | ( | uint8_t | gpio_label, |
uint8_t | gpio_mode, |
||
uint32_t * | value |
||
) |
Send a request to read or write a GPIO.
- Parameters
-
gpio_label
is the GPIO label to control (defined in the PDS) gpio_mode
defines how to read or set the GPIO value
returns the read value or the detailed error cause
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line 1302
of file sl_wfx.c
.
References sl_wfx_control_gpio_req_body_t::gpio_label
, sl_wfx_control_gpio_req_body_t::gpio_mode
, SL_WFX_CONTROL_GPIO_REQ_ID
, sl_wfx_get_status_code()
, sl_wfx_send_command()
, and SL_WFX_STA_INTERFACE
.
◆ sl_wfx_prevent_rollback()
sl_status_t sl_wfx_prevent_rollback | ( | uint32_t | magic_word | ) |
Prevent Rollback request.
- Parameters
-
magic_word
Used to prevent mistakenly sent request from burning the OTP
- Returns
- SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Definition at line 1475
of file sl_wfx.c
.
References sl_wfx_prevent_rollback_req_body_t::magic_word
, SL_WFX_PREVENT_ROLLBACK_REQ_ID
, sl_wfx_send_command()
, and SL_WFX_STA_INTERFACE
.
◆ sl_wfx_pta_priority()
sl_status_t sl_wfx_pta_priority | ( | uint32_t | priority | ) |
Send a request to define the level of priority used to arbitrate concurrent Coex and Wlan requests.
- Parameters
-
priority
defines the priority levels for concurrent Coex and WLAN request arbitration - SL_WFX_PTA_PRIORITY_COEX_MAXIMIZED
- SL_WFX_PTA_PRIORITY_COEX_HIGH
- SL_WFX_PTA_PRIORITY_BALANCED
- SL_WFX_PTA_PRIORITY_WLAN_HIGH
- SL_WFX_PTA_PRIORITY_WLAN_MAXIMIZED
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line 1412
of file sl_wfx.c
.
References sl_wfx_pta_priority_req_body_t::priority
, SL_WFX_PTA_PRIORITY_REQ_ID
, sl_wfx_send_command()
, and SL_WFX_STA_INTERFACE
.
◆ sl_wfx_pta_settings()
sl_status_t sl_wfx_pta_settings | ( | uint8_t | pta_mode, |
uint8_t | request_signal_active_level, |
||
uint8_t | priority_signal_active_level, |
||
uint8_t | freq_signal_active_level, |
||
uint8_t | grant_signal_active_level, |
||
uint8_t | coex_type, |
||
uint8_t | default_grant_state, |
||
uint8_t | simultaneous_rx_access, |
||
uint8_t | priority_sampling_time, |
||
uint8_t | tx_rx_sampling_time, |
||
uint8_t | freq_sampling_time, |
||
uint8_t | grant_valid_time, |
||
uint8_t | fem_control_time, |
||
uint8_t | first_slot_time, |
||
uint16_t | periodic_tx_rx_sampling_time, |
||
uint16_t | coex_quota, |
||
uint16_t | wlan_quota |
||
) |
Send a request to set the PTA mode, the active levels on signals, the Coex type, to define the timings, quotas, combined mode and default grant state.
- Parameters
-
pta_mode
defines the mode to use - SL_WFX_PTA_1W_WLAN_MASTER
- SL_WFX_PTA_1W_COEX_MASTER
- SL_WFX_PTA_2W
- SL_WFX_PTA_3W
- SL_WFX_PTA_4W
request_signal_active_level
is the active level on REQUEST signal (PTA_RF_ACT pin) priority_signal_active_level
is the active level on PRIORITY signal (PTA_STATUS pin) freq_signal_active_level
is the active level on FREQ signal (PTA_FREQ pin) grant_signal_active_level
is the active level on GRANT signal (PTA_TX_CONF pin) - SL_WFX_SIGNAL_LOW
- SL_WFX_SIGNAL_HIGH
coex_type
- SL_WFX_COEX_TYPE_GENERIC
- SL_WFX_COEX_TYPE_BLE
default_grant_state
is the state of the GRANT signal before arbitration at grant_valid_time - SL_WFX_NO_GRANT
- SL_WFX_GRANT
simultaneous_rx_access
is a boolean to allow both Coex and Wlan to receive concurrently, also named combined mode priority_sampling_time
is the time (in microseconds) from the Coex request to the sampling of the priority on PRIORITY signal (1 to 31) tx_rx_sampling_time
is the time (in microseconds) from the Coex request to the sampling of the directionality on PRIORITY signal (priority_sampling_time to 63) freq_sampling_time
is the time (in microseconds) from the Coex request to the sampling of freq-match information on FREQ signal (1 to 127) grant_valid_time
is the time (in microseconds) from Coex request to the GRANT signal assertion (MAX(tx_rx_sampling_time, freq_sampling_time) to 255) fem_control_time
is the time (in microseconds) from Coex request to the control of FEM (grant_valid_time to 255) first_slot_time
is the time (in microseconds) from the Coex request to the beginning of reception or transmission (grant_valid_time to 255) periodic_tx_rx_sampling_time
is the period (in microseconds) from first_slot_time of following samplings of the directionality on PRIORITY signal (1 to 1023) coex_quota
is the duration (in microseconds) for which RF is granted to Coex before it is moved to Wlan wlan_quota
is the duration (in microseconds) for which RF is granted to Wlan before it is moved to Coex
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line 1356
of file sl_wfx.c
.
References sl_wfx_pta_settings_req_body_t::coex_quota
, sl_wfx_pta_settings_req_body_t::coex_type
, sl_wfx_pta_settings_req_body_t::default_grant_state
, sl_wfx_pta_settings_req_body_t::fem_control_time
, sl_wfx_pta_settings_req_body_t::first_slot_time
, sl_wfx_pta_settings_req_body_t::freq_sampling_time
, sl_wfx_pta_settings_req_body_t::freq_signal_active_level
, sl_wfx_pta_settings_req_body_t::grant_signal_active_level
, sl_wfx_pta_settings_req_body_t::grant_valid_time
, sl_wfx_pta_settings_req_body_t::periodic_tx_rx_sampling_time
, sl_wfx_pta_settings_req_body_t::priority_sampling_time
, sl_wfx_pta_settings_req_body_t::priority_signal_active_level
, sl_wfx_pta_settings_req_body_t::pta_mode
, sl_wfx_pta_settings_req_body_t::request_signal_active_level
, sl_wfx_pta_settings_req_body_t::simultaneous_rx_access
, SL_WFX_PTA_SETTINGS_REQ_ID
, sl_wfx_send_command()
, SL_WFX_STA_INTERFACE
, sl_wfx_pta_settings_req_body_t::tx_rx_sampling_time
, and sl_wfx_pta_settings_req_body_t::wlan_quota
.
◆ sl_wfx_pta_state()
sl_status_t sl_wfx_pta_state | ( | uint32_t | pta_state | ) |
Send a request to start or stop the PTA.
- Parameters
-
pta_state
defines the requested state of the PTA - SL_WFX_PTA_OFF
- SL_WFX_PTA_ON
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line 1433
of file sl_wfx.c
.
References sl_wfx_pta_state_req_body_t::pta_state
, SL_WFX_PTA_STATE_REQ_ID
, sl_wfx_send_command()
, and SL_WFX_STA_INTERFACE
.
◆ sl_wfx_secure_link_configure()
sl_status_t sl_wfx_secure_link_configure | ( | const uint8_t * | encryption_bitmap, |
uint8_t | disable_session_key_protection |
||
) |
Modify SecureLink configuration.
- Parameters
-
encryption_bitmap
Encryption bitmap that must be written to wf200 disable_session_key_protection
Force the firmware to authorize the use of the same session key during a complete power cycle, even very long.
- Note
- Disabling the session key protection downgrades the link security and is NOT RECOMMENDED.
- The magic word SL_WFX_SESSION_KEY_PROTECTION_DISABLE_MAGIC is used to disable this protection.
- Returns
- Returns SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
- Note
- The bitmap used as a parameter will be copied to the context bitmap if the setting completed successfully.
Definition at line 247
of file sl_wfx_secure_link.c
.
References sl_wfx_securelink_configure_req_body_t::encr_bmp
.
◆ sl_wfx_secure_link_exchange_keys()
sl_status_t sl_wfx_secure_link_exchange_keys | ( | const uint8_t * | sl_mac_key, |
uint8_t * | sl_host_pub_key |
||
) |
Exchange SecureLink public keys.
- Parameters
-
sl_mac_key
MAC key to be used sl_host_pub_key
public key of the host
- Returns
- Returns SL_STATUS_OK if the request has been sent correctly, SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED otherwise
Definition at line 139
of file sl_wfx_secure_link.c
.
References sl_wfx_allocate_command_buffer()
, and SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_REQ_ID
.
◆ sl_wfx_secure_link_renegotiate_session_key()
sl_status_t sl_wfx_secure_link_renegotiate_session_key | ( | void |
| ) |
Renegotiate session key request.
- Returns
- SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Definition at line 183
of file sl_wfx_secure_link.c
.
◆ sl_wfx_secure_link_set_mac_key()
sl_status_t sl_wfx_secure_link_set_mac_key | ( | const uint8_t * | sl_mac_key, |
sl_wfx_securelink_mac_key_dest_t | destination |
||
) |
SecureLink Set MAC Key.
- Parameters
-
sl_mac_key
MAC key to write on wf200 destination
Memory section where it should be written - SL_MAC_KEY_DEST_OTP
- SL_MAC_KEY_DEST_RAM
- Returns
- Returns SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line 113
of file sl_wfx_secure_link.c
.
References sl_wfx_set_securelink_mac_key_req_body_t::key_value
, and sl_wfx_set_securelink_mac_key_req_body_t::otp_or_ram
.
◆ sl_wfx_send_configuration()
sl_status_t sl_wfx_send_configuration | ( | const char * | pds_data, |
uint32_t | pds_data_length |
||
) |
Function to send PDS chunks.
- Parameters
-
pds_data
Data to be sent in the compressed PDS format pds_data_length
Size of the data to be sent
- Returns
- SL_STATUS_OK if the configuration has been sent correctly, SL_STATUS_FAIL otherwise
- Note
- The PDS (Platform Data Set) file contains the WF200 settings
Definition at line 1255
of file sl_wfx.c
.
References sl_wfx_allocate_command_buffer()
, and SL_WFX_CONFIGURATION_REQ_ID
.
Referenced by sl_wfx_set_antenna_config()
.
◆ sl_wfx_set_cca_config()
sl_status_t sl_wfx_set_cca_config | ( | uint8_t | cca_thr_mode | ) |
Send a request to configure the CCA mode.
- Parameters
-
cca_thr_mode
defines the requested mode for CCA - SL_WFX_CCA_THR_MODE_RELATIVE
- SL_WFX_CCA_THR_MODE_ABSOLUTE
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line 1454
of file sl_wfx.c
.
References sl_wfx_set_cca_config_req_body_t::cca_thr_mode
, sl_wfx_set_cca_config_req_body_t::reserved
, sl_wfx_send_command()
, SL_WFX_SET_CCA_CONFIG_REQ_ID
, and SL_WFX_STA_INTERFACE
.
◆ sl_wfx_shutdown()
sl_status_t sl_wfx_shutdown | ( | void |
| ) |
Shutdown the Wi-Fi chip.
- Returns
- SL_STATUS_OK if the Wi-Fi chip has been shutdown correctly, SL_STATUS_FAIL otherwise
- Note
- Send the shutdown command, clear the WUP bit and the GPIO WUP to enable the Wi-Fi chips to go to sleep
Definition at line 1493
of file sl_wfx.c
.
References sl_wfx_allocate_command_buffer()
, and SL_WFX_SHUT_DOWN_REQ_ID
.
Referenced by sl_wfx_deinit()
.