sl_wfx_context_t Struct Reference

Structure used to maintain the Wi-Fi solution context on the host side.

Data Fields

uint8_t event_payload_buffer [512]
 Event payload associated with the last posted event.
 
uint8_t firmware_build
 Firmware build version.
 
uint8_t firmware_minor
 Firmware minor version.
 
uint8_t firmware_major
 Firmware major version.
 
uint16_t data_frame_id
 Frame ID incremented by sl_wfx_send_ethernet_frame.
 
uint16_t used_buffers
 Number of buffers currently in use by the WFx chip.
 
uint8_t wfx_opn [14]
 OPN of the part.
 
sl_wfx_mac_address_t mac_addr_0
 Mac address used by WFx interface 0, station.
 
sl_wfx_mac_address_t mac_addr_1
 Mac address used by WFx interface 1, softap.
 
sl_wfx_state_t state
 State of the WFx Wi-Fi chip.

Structure used to maintain the Wi-Fi solution context on the host side.

Definition at line 400 of file sl_wfx_constants.h.

Field Documentation

◆ data_frame_id

uint16_t sl_wfx_context_t::data_frame_id

Frame ID incremented by sl_wfx_send_ethernet_frame.

Definition at line 405 of file sl_wfx_constants.h.

Referenced by sl_wfx_send_ethernet_frame().

◆ event_payload_buffer

uint8_t sl_wfx_context_t::event_payload_buffer[512]

Event payload associated with the last posted event.

Definition at line 401 of file sl_wfx_constants.h.

◆ firmware_build

uint8_t sl_wfx_context_t::firmware_build

Firmware build version.

Definition at line 402 of file sl_wfx_constants.h.

Referenced by sl_wfx_init().

◆ firmware_major

uint8_t sl_wfx_context_t::firmware_major

Firmware major version.

Definition at line 404 of file sl_wfx_constants.h.

Referenced by sl_wfx_init().

◆ firmware_minor

uint8_t sl_wfx_context_t::firmware_minor

Firmware minor version.

Definition at line 403 of file sl_wfx_constants.h.

Referenced by sl_wfx_init().

◆ mac_addr_0

sl_wfx_mac_address_t sl_wfx_context_t::mac_addr_0

Mac address used by WFx interface 0, station.

Definition at line 408 of file sl_wfx_constants.h.

Referenced by sl_wfx_init(), and sl_wfx_set_mac_address().

◆ mac_addr_1

sl_wfx_mac_address_t sl_wfx_context_t::mac_addr_1

Mac address used by WFx interface 1, softap.

Definition at line 409 of file sl_wfx_constants.h.

Referenced by sl_wfx_init(), and sl_wfx_set_mac_address().

◆ state

sl_wfx_state_t sl_wfx_context_t::state

State of the WFx Wi-Fi chip.

Definition at line 410 of file sl_wfx_constants.h.

Referenced by sl_wfx_disable_device_power_save(), and sl_wfx_enable_device_power_save().

◆ used_buffers

uint16_t sl_wfx_context_t::used_buffers

Number of buffers currently in use by the WFx chip.

Definition at line 406 of file sl_wfx_constants.h.

Referenced by sl_wfx_init(), and sl_wfx_send_request().

◆ wfx_opn

uint8_t sl_wfx_context_t::wfx_opn[14]

OPN of the part.

Definition at line 407 of file sl_wfx_constants.h.

Referenced by sl_wfx_get_opn(), and sl_wfx_init().


The documentation for this struct was generated from the following file:
  • sl_wfx_constants.h