sl_wfx_mac_address_t Struct Reference
Structure to handle MAC address format.
Data Fields | |
uint8_t | octet [6] |
Table to store a MAC address. |
Structure to handle MAC address format.
Definition at line 363
of file sl_wfx_constants.h
.
Field Documentation
◆ octet
uint8_t sl_wfx_mac_address_t::octet[6] |
Table to store a MAC address.
Definition at line 364
of file sl_wfx_constants.h
.
Referenced by sl_wfx_add_blacklist_address()
, sl_wfx_add_multicast_address()
, sl_wfx_add_whitelist_address()
, sl_wfx_disconnect_ap_client_command()
, sl_wfx_get_ap_client_signal_strength()
, sl_wfx_init()
, sl_wfx_remove_multicast_address()
, and sl_wfx_set_mac_address()
.
The documentation for this struct was generated from the following file:
sl_wfx_constants.h