sl_wfx_nonce_t Struct Reference
Structure to maintain secure link counters.
Data Fields | |
uint32_t | hp_packet_count |
High priority packet counter. | |
uint32_t | rx_packet_count |
Received packet counter. | |
uint32_t | tx_packet_count |
Sent packet counter. |
Structure to maintain secure link counters.
Definition at line 379
of file sl_wfx_constants.h
.
Field Documentation
◆ hp_packet_count
uint32_t sl_wfx_nonce_t::hp_packet_count |
High priority packet counter.
Definition at line 380
of file sl_wfx_constants.h
.
◆ rx_packet_count
uint32_t sl_wfx_nonce_t::rx_packet_count |
Received packet counter.
Definition at line 381
of file sl_wfx_constants.h
.
◆ tx_packet_count
uint32_t sl_wfx_nonce_t::tx_packet_count |
Sent packet counter.
Definition at line 382
of file sl_wfx_constants.h
.
The documentation for this struct was generated from the following file:
sl_wfx_constants.h