Enabling Wireless Extension Tools#
Wireless Extension tools, such as 'iwconfig' and 'iwpriv' are required for configuring the driver. Make sure that the wireless extensions are enabled in the Linux kernel configuration file.
Enable these options in the kernel configuration file, re-compile the kernel, and cross compile the driver.
CONFIG_WIRELESS
CONFIG_WIRELESS_EXT
CONFIG_WEXT_PRIV
CONFIG_WEXT_SPY
CONFIG_WEXT_PROC
CONFIG_WEXT_CORE
CONFIG_HOSTAPSee the Kernel Configuration section for the commands to compile the kernel.