Public Attributes#
uint8_t, Advertising SID subfield in the ADI field used to identify the Periodic Advertising.
uint8_t, Advertiser Address Type, this parameter indicates the type of address being used in the connection request packets
uint8_t, Advertiser Address[6]
uint16_t, Skip,The maximum number of periodic advertising events that can be skipped after a successful receive Range : 0x0000 to 0x01F3
uint16_t, Sync Timeout, Synchronization timeout for the periodic advertising train Range : 0x000A to 0x4000
Public Attribute Documentation#
fil_policy#
uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::fil_policy
1353
of file components/si91x/ble/inc/rsi_ble.h
adv_sid#
uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::adv_sid
uint8_t, Advertising SID subfield in the ADI field used to identify the Periodic Advertising.
Range : 0x00 to 0x0F, All other bits - Reserved for future use
1357
of file components/si91x/ble/inc/rsi_ble.h
adv_addr_type#
uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::adv_addr_type
uint8_t, Advertiser Address Type, this parameter indicates the type of address being used in the connection request packets
0x00 Public Device Address or Public Identity Address
0x01 Random Device Address or Random (static) Identity Address
All other values Reserved for future use
1364
of file components/si91x/ble/inc/rsi_ble.h
adv_addr#
uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::adv_addr[RSI_DEV_ADDR_LEN]
uint8_t, Advertiser Address[6]
1366
of file components/si91x/ble/inc/rsi_ble.h
skip#
uint16_t rsi_ble_ae_set_periodic_adv_create_sync_s::skip
uint16_t, Skip,The maximum number of periodic advertising events that can be skipped after a successful receive Range : 0x0000 to 0x01F3
1369
of file components/si91x/ble/inc/rsi_ble.h
sync_timeout#
uint16_t rsi_ble_ae_set_periodic_adv_create_sync_s::sync_timeout
uint16_t, Sync Timeout, Synchronization timeout for the periodic advertising train Range : 0x000A to 0x4000
1372
of file components/si91x/ble/inc/rsi_ble.h
reserved#
uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::reserved
1373
of file components/si91x/ble/inc/rsi_ble.h