You are viewing documentation for version:3.0.13Public Attributes#uint8_tdev_addr_typeuint8_tdev_addruint8_tfilter_policyuint8_town_addr_typeuint16_tle_scan_intervaluint16_tle_scan_windowuint16_tconn_interval_minuint16_tconn_interval_maxuint16_tconn_latencyuint16_tsupervision_toutuint16_tmin_ce_lengthuint16_tmax_ce_lengthPublic Attribute Documentation#dev_addr_type#uint8_t rsi_ble_req_enhance_conn_s::dev_addr_typedev_addr#uint8_t rsi_ble_req_enhance_conn_s::dev_addr[RSI_DEV_ADDR_LEN]filter_policy#uint8_t rsi_ble_req_enhance_conn_s::filter_policyown_addr_type#uint8_t rsi_ble_req_enhance_conn_s::own_addr_typele_scan_interval#uint16_t rsi_ble_req_enhance_conn_s::le_scan_intervalle_scan_window#uint16_t rsi_ble_req_enhance_conn_s::le_scan_windowconn_interval_min#uint16_t rsi_ble_req_enhance_conn_s::conn_interval_minconn_interval_max#uint16_t rsi_ble_req_enhance_conn_s::conn_interval_maxconn_latency#uint16_t rsi_ble_req_enhance_conn_s::conn_latencysupervision_tout#uint16_t rsi_ble_req_enhance_conn_s::supervision_toutmin_ce_length#uint16_t rsi_ble_req_enhance_conn_s::min_ce_lengthmax_ce_length#uint16_t rsi_ble_req_enhance_conn_s::max_ce_length