You are viewing documentation for version:3.0.13Public Attributes#uint8_tdev_addruint16_tmin_intervaluint16_tmax_intervaluint16_tlatencyuint16_ttimeoutPublic Attribute Documentation#dev_addr#uint8_t rsi_ble_cmd_conn_params_update_s::dev_addr[RSI_DEV_ADDR_LEN]min_interval#uint16_t rsi_ble_cmd_conn_params_update_s::min_intervalmax_interval#uint16_t rsi_ble_cmd_conn_params_update_s::max_intervallatency#uint16_t rsi_ble_cmd_conn_params_update_s::latencytimeout#uint16_t rsi_ble_cmd_conn_params_update_s::timeout