Public Attributes#

uint8_t

Scanning Status 0 - disable 1 - enable.

uint8_t

Scanning type #define SCAN_TYPE_ACTIVE 0x01 #define SCAN_TYPE_PASSIVE 0x00.

uint8_t

To filter incoming advertising reports FILTERING_DISABLED = 0 (default) WHITELIST_FILTERING = 1.

uint8_t

Address type of the local device #define LE_PUBLIC_ADDRESS 0x00 #define LE_RANDOM_ADDRESS 0x01 #define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02 #define LE_RESOLVABLE_RANDOM_ADDRESS 0x03

uint16_t

Scan interval This is defined as the time interval from when the Controller started its last LE scan until it begins the subsequent LE scan.

uint16_t

Scan window The duration of the LE scan.

Public Attribute Documentation#

status#

uint8_t rsi_ble_req_scan_s::status

Scanning Status 0 - disable 1 - enable.


scan_type#

uint8_t rsi_ble_req_scan_s::scan_type

Scanning type #define SCAN_TYPE_ACTIVE 0x01 #define SCAN_TYPE_PASSIVE 0x00.


filter_type#

uint8_t rsi_ble_req_scan_s::filter_type

To filter incoming advertising reports FILTERING_DISABLED = 0 (default) WHITELIST_FILTERING = 1.

Note


own_addr_type#

uint8_t rsi_ble_req_scan_s::own_addr_type

Address type of the local device #define LE_PUBLIC_ADDRESS 0x00 #define LE_RANDOM_ADDRESS 0x01 #define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02 #define LE_RESOLVABLE_RANDOM_ADDRESS 0x03


scan_int#

uint16_t rsi_ble_req_scan_s::scan_int

Scan interval This is defined as the time interval from when the Controller started its last LE scan until it begins the subsequent LE scan.

Range: 0x0004 to 0x4000


scan_win#

uint16_t rsi_ble_req_scan_s::scan_win

Scan window The duration of the LE scan.

LE_Scan_Window shall be less than or equal to LE_Scan_Interval Range: 0x0004 to 0x4000