Structure to hold the parameters of timer OCU control parameters like compare values, DMA state.
Public Attributes#
boolean_t
CT counter number sl_counter_number_t.
boolean_t
DMA state for counter, true to enable and false to disable it.
pointer to OCU control parameters structure
pointer to MCPWM callback structure
Public Attribute Documentation#
is_counter_number_1#
boolean_t sl_config_timer_ocu_control_t::is_counter_number_1
CT counter number sl_counter_number_t.
Definition at line
246
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_config_timer.h
is_dma_state_enabled#
boolean_t sl_config_timer_ocu_control_t::is_dma_state_enabled
DMA state for counter, true to enable and false to disable it.
Definition at line
247
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_config_timer.h
params#
sl_config_timer_ocu_params_t* sl_config_timer_ocu_control_t::params
pointer to OCU control parameters structure
Definition at line
248
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_config_timer.h
callback#
sl_config_timer_pwm_callback_t* sl_config_timer_ocu_control_t::callback
pointer to MCPWM callback structure
Definition at line
249
of file components/siwx917_soc/drivers/unified_api/inc/sl_si91x_config_timer.h