Structure to hold portl and pinh for channels.

Public Attributes#

uint8_t

PWM GPIO output low side port.

uint8_t

PWM GPIO output low side pin.

uint8_t

PWM GPIO output high side port.

uint8_t

PWM GPIO output high side pin.

uint8_t

PWM GPIO output low side mux.

uint8_t

PWM GPIO output high side mux.

uint8_t

PWM GPIO output low side pad.

uint8_t

PWM GPIO output high side pad.

Public Attribute Documentation#

port_l#

uint8_t sl_pwm_init_t::port_l

PWM GPIO output low side port.


Definition at line 264 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

pin_l#

uint8_t sl_pwm_init_t::pin_l

PWM GPIO output low side pin.


Definition at line 265 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

port_h#

uint8_t sl_pwm_init_t::port_h

PWM GPIO output high side port.


Definition at line 266 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

pin_h#

uint8_t sl_pwm_init_t::pin_h

PWM GPIO output high side pin.


Definition at line 267 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

mux_l#

uint8_t sl_pwm_init_t::mux_l

PWM GPIO output low side mux.


Definition at line 268 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

mux_h#

uint8_t sl_pwm_init_t::mux_h

PWM GPIO output high side mux.


Definition at line 269 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

pad_l#

uint8_t sl_pwm_init_t::pad_l

PWM GPIO output low side pad.


Definition at line 270 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

pad_h#

uint8_t sl_pwm_init_t::pad_h

PWM GPIO output high side pad.


Definition at line 271 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h