typedef for SSI control config struct

Public Attributes#

uint8_t

bit width either 8 or 16 bit

uint32_t

mode such as Master or Slave mode

uint32_t

clock mode such as CPOL0 CPHA1

uint32_t

baud rate for SSI

uint32_t

Delay for receive input signal.

Public Attribute Documentation#

bit_width#

uint8_t sl_ssi_control_config_t::bit_width

bit width either 8 or 16 bit


device_mode#

uint32_t sl_ssi_control_config_t::device_mode

mode such as Master or Slave mode


clock_mode#

uint32_t sl_ssi_control_config_t::clock_mode

clock mode such as CPOL0 CPHA1


baud_rate#

uint32_t sl_ssi_control_config_t::baud_rate

baud rate for SSI


receive_sample_delay#

uint32_t sl_ssi_control_config_t::receive_sample_delay

Delay for receive input signal.