Structure to hold the parameters of timer clock-source configurations.

Public Attributes#

uint8_t

true to enable static and false to enable dynamic clock type

boolean_t

true to enable and false to disable ULP timer in synchronous mode to ULPSS pclk

uint8_t

timer input clock source, refer ulp_timer_clk_input_source_t for possible values

boolean_t

true to wait and false to Skip waiting for switching timer clk

Public Attribute Documentation#

ulp_timer_clk_type#

uint8_t ulp_timer_clk_src_config_t::ulp_timer_clk_type

true to enable static and false to enable dynamic clock type


Definition at line 102 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h

ulp_timer_sync_to_ulpss_pclk#

boolean_t ulp_timer_clk_src_config_t::ulp_timer_sync_to_ulpss_pclk

true to enable and false to disable ULP timer in synchronous mode to ULPSS pclk


Definition at line 104 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h

ulp_timer_clk_input_src#

uint8_t ulp_timer_clk_src_config_t::ulp_timer_clk_input_src

timer input clock source, refer ulp_timer_clk_input_source_t for possible values


Definition at line 106 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h

ulp_timer_skip_switch_time#

boolean_t ulp_timer_clk_src_config_t::ulp_timer_skip_switch_time

true to wait and false to Skip waiting for switching timer clk


Definition at line 107 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h