Structure to hold the clock configuration parameters.

Public Attributes#

uint8_t

SoC PLL count value.

uint16_t

Int PLL control value.

uint32_t

Intf PLL clock frequency.

uint32_t

Intf PLL reference clock frequency.

uint32_t

SoC PLL clock frequency.

uint32_t

SoC PLL reference clock frequency.

uint16_t

Clock Division Factor.

Public Attribute Documentation#

soc_pll_mm_count_value#

uint8_t sl_gspi_clock_config_t::soc_pll_mm_count_value

SoC PLL count value.


Definition at line 117 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h

intf_pll_500_control_value#

uint16_t sl_gspi_clock_config_t::intf_pll_500_control_value

Int PLL control value.


Definition at line 118 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h

intf_pll_clock#

uint32_t sl_gspi_clock_config_t::intf_pll_clock

Intf PLL clock frequency.


Definition at line 119 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h

intf_pll_reference_clock#

uint32_t sl_gspi_clock_config_t::intf_pll_reference_clock

Intf PLL reference clock frequency.


Definition at line 120 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h

soc_pll_clock#

uint32_t sl_gspi_clock_config_t::soc_pll_clock

SoC PLL clock frequency.


Definition at line 121 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h

soc_pll_reference_clock#

uint32_t sl_gspi_clock_config_t::soc_pll_reference_clock

SoC PLL reference clock frequency.


Definition at line 122 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h

division_factor#

uint16_t sl_gspi_clock_config_t::division_factor

Clock Division Factor.


Definition at line 123 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h