You are viewing documentation for version:
Structure to hold the parameters of timer configurations. 
Public Attributes#
uint8_t
timer number, SL_ULP_TIMER_NUMBER for default values 
uint8_t
timer mode, SL_ULP_TIMER_MODE for default values 
uint8_t
timer type, SL_ULP_TIMER_TYPE for default values 
uint32_t
timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds 
uint8_t
timer direction, SL_ULP_TIMER_DIRECTION for default values 
Public Attribute Documentation#
timer_num#
uint8_t ulp_timer_config_t::timer_num
timer number, SL_ULP_TIMER_NUMBER for default values 
timer_mode#
uint8_t ulp_timer_config_t::timer_mode
timer mode, SL_ULP_TIMER_MODE for default values 
timer_type#
uint8_t ulp_timer_config_t::timer_type
timer type, SL_ULP_TIMER_TYPE for default values 
timer_match_value#
uint32_t ulp_timer_config_t::timer_match_value
timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds 
timer_direction#
uint8_t ulp_timer_config_t::timer_direction
timer direction, SL_ULP_TIMER_DIRECTION for default values