Analog to Digital Converter#
Modules#
Enumerations#
Enumeration for ADC input type.
Enumeration for ADC operation mode.
Enumeration for ADC DMA type.
Enumeration for ADC multiple channel selection.
Enumeration for ADC external trigger type.
Enumeration for ADC external trigger number.
Enumeration for ADC external trigger edge selection.
Enumeration for ADC external trigger selection.
Enumeration for ADC channel.
Typedefs#
Renamed ADC channel configuration structure.
Renamed ADC configuration structure.
Renamed ADC internal configuration structure.
Renamed ADC external trigger configuration structure.
Typedef for user supplied callback function, which is called when ADC sample completes.
Functions#
Set the clock for the ADC peripheral, Configures the PLL clock with the value set by user in the clock configuration structure.
Initialize the ADC peripheral.
Configure ADC channel parameters.
Register the user callback function.
Un-register the user callback function.
Configure the ADC external trigger.
Configure the ADC sampling rate for the ADC channels.
ADC can give a sample for the selected trigger with a trigger match.
Clear the ADC external trigger.
Configure the ADC ping and pong memory location and length To configure the Ping and pong memory location along with length of ping memory and pong memory.
Enable ping pong for the corresponding ADC channels It is an applicable only for FIFO mode of ADC operation.
Disable ping pong for the corresponding ADC channels.
Enable DMA for the corresponding ADC channels.
Disable DMA for the corresponding ADC channels.
Configure the ADC in Static Mode it can be programmed for setting input type, positive and negative input channel selection.
Configure the ADC in FIFO Mode.
Enable the ADC channel.
Disable the ADC channel.
Set the Power On and off for ADC.
Enable or Disable the Noise averaging mode to ADC.
Enable BJT based Temperature sensor as an input to ADC.
Configuring ADC fifo threshold.
Configure the ADC threshold to compare threshold value with ADC data.
Read the ADC samples when FIFO mode is enabled.
Read the ADC samples when static mode is enabled.
To get the channel sampling rate value which is configured to ADC.
Uninitialize the ADC.
Start the ADC operation.
Stop the ADC operation.
Get the ADC version.
Macros#
Enumeration Documentation#
sl_adc_input_type_typedef_t#
sl_adc_input_type_typedef_t
Enumeration for ADC input type.
| Enumerator | |
|---|---|
| SL_ADC_SINGLE_ENDED | Input type single ended. |
| SL_ADC_DIFFERENTIAL | Input type differential. |
| SL_ADC_INPUT_TYPE_LAST | Last member of enum for validation. |
sl_adc_operation_mode_typedef_t#
sl_adc_operation_mode_typedef_t
Enumeration for ADC operation mode.
| Enumerator | |
|---|---|
| SL_ADC_FIFO_MODE | operation mode as fifo mode |
| SL_ADC_STATIC_MODE | operation mode as static mode |
| SL_ADC_OPERATION_MODE_LAST | Last member of enum for validation. |
sl_adc_dma_type_typedef_t#
sl_adc_dma_type_typedef_t
Enumeration for ADC DMA type.
| Enumerator | |
|---|---|
| SL_ADC_INTERNAL_DMA | Internal DMA type. |
| SL_ADC_EXTERNAL_DMA | External DMA type. |
| SL_ADC_DMA_TYPE_LAST | Last member of enum for validation. |
sl_adc_channel_type_typedef_t#
sl_adc_channel_type_typedef_t
Enumeration for ADC multiple channel selection.
| Enumerator | |
|---|---|
| SL_ADC_SINGLE_CHNL | Dynamic mode disable. |
| SL_ADC_MULTI_CHNL | Dynamic mode enable. |
| SL_ADC_CHANNEL_TYPE_LAST | Last member of enum for validation. |
sl_adc_ext_trigger_type_t#
sl_adc_ext_trigger_type_t
Enumeration for ADC external trigger type.
| Enumerator | |
|---|---|
| SL_ULP_TIMER_EXT_TRIGGER | ULP timer external trigger type. |
| SL_ULP_GPIO_EXT_TRIGGER | ULP gpio external trigger type. |
| SL_M4_CT_EXT_TRIGGER | M4 CT external trigger type. |
| SL_ADC_EXT_TRIGGER_TYPE_LAST | Last member of enum for validation. |
sl_adc_ext_trigger_num_t#
sl_adc_ext_trigger_num_t
Enumeration for ADC external trigger number.
| Enumerator | |
|---|---|
| SL_ADC_EXT_TRIGGER_1 | External trigger detection 1. |
| SL_ADC_EXT_TRIGGER_2 | External trigger detection 2. |
| SL_ADC_EXT_TRIGGER_3 | External trigger detection 3. |
| SL_ADC_EXT_TRIGGER_4 | External trigger detection 4. |
| SL_ADC_EXT_TRIGGER_LAST | Last member of enum for validation. |
sl_adc_ext_trigger_edge_t#
sl_adc_ext_trigger_edge_t
Enumeration for ADC external trigger edge selection.
| Enumerator | |
|---|---|
| SL_ADC_EXT_TRIGGER_POS_EDGE | External trigger positive edge. |
| SL_ADC_EXT_TRIGGER_NEG_EDGE | External trigger negative edge. |
| SL_ADC_EXT_TRIGGER_POS_NEG_EDGE | External trigger positive and negative edge. |
| SL_ADC_EXT_TRIGGER_EDGE_LAST | Last member of enum for validation. |
sl_adc_ext_trigger_sel_t#
sl_adc_ext_trigger_sel_t
Enumeration for ADC external trigger selection.
| Enumerator | |
|---|---|
| SL_ADC_EXT_TRIGGER_SEL_1 | External trigger selection 1. |
| SL_ADC_EXT_TRIGGER_SEL_2 | External trigger selection 2. |
| SL_ADC_EXT_TRIGGER_SEL_3 | External trigger selection 3. |
| SL_ADC_EXT_TRIGGER_SEL_4 | External trigger selection 4. |
| SL_ADC_EXT_TRIGGER_SEL_LAST | Last member of enum for validation. |
sl_adc_channel_id_t#
sl_adc_channel_id_t
Enumeration for ADC channel.
| Enumerator | |
|---|---|
| SL_ADC_CHANNEL_0 | ADC channel 1. |
| SL_ADC_CHANNEL_1 | ADC channel 2. |
| SL_ADC_CHANNEL_2 | ADC channel 3. |
| SL_ADC_CHANNEL_3 | ADC channel 4. |
| SL_ADC_CHANNEL_4 | ADC channel 5. |
| SL_ADC_CHANNEL_5 | ADC channel 6. |
| SL_ADC_CHANNEL_6 | ADC channel 7. |
| SL_ADC_CHANNEL_7 | ADC channel 8. |
| SL_ADC_CHANNEL_8 | ADC channel 9. |
| SL_ADC_CHANNEL_9 | ADC channel 10. |
| SL_ADC_CHANNEL_10 | ADC channel 11. |
| SL_ADC_CHANNEL_11 | ADC channel 12. |
| SL_ADC_CHANNEL_12 | ADC channel 13. |
| SL_ADC_CHANNEL_13 | ADC channel 14. |
| SL_ADC_CHANNEL_14 | ADC channel 15. |
| SL_ADC_CHANNEL_15 | ADC channel 16. |
Typedef Documentation#
sl_adc_channel_config_t#
typedef adc_ch_config_t sl_adc_channel_config_t
Renamed ADC channel configuration structure.
sl_adc_internal_config_t#
typedef adc_inter_config_t sl_adc_internal_config_t
Renamed ADC internal configuration structure.
sl_adc_external_config_t#
typedef adc_extr_config_t sl_adc_external_config_t
Renamed ADC external trigger configuration structure.
sl_adc_callback_t#
typedef void(* sl_adc_callback_t) (uint8_t channel, uint8_t event) )(uint8_t channel, uint8_t event)
Typedef for user supplied callback function, which is called when ADC sample completes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | channel | ADC channel number | |
| [in] | event | ADC event for different interrupt. |
Function Documentation#
sl_si91x_adc_configure_clock#
sl_status_t sl_si91x_adc_configure_clock (sl_adc_clock_config_t * clock_configuration)
Set the clock for the ADC peripheral, Configures the PLL clock with the value set by user in the clock configuration structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_clock_config_t * | [in] | clock_configuration | : clock structure variables ( sl_adc_clock_config_t) |
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_FAIL (0x0001) - The function is failed
SL_STATUS_NOT_INITIALIZED (0x0011) - Clock is not initialized
sl_si91x_adc_init#
sl_status_t sl_si91x_adc_init (sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config, float vref_value)
Initialize the ADC peripheral.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_channel_config_t | [in] | adc_channel_config | : ADC channels configuration structure variable |
| sl_adc_config_t | [in] | adc_config | : ADC operation configuration structure variable |
| float | [in] | vref_value | : Reference voltage |
Based on the sampling rate, the ADC clock source will set and Pass the Vref value to set the reference voltage to ADC.
Pre-conditions:
sl_si91x_adc_configure_clock - Only for FIFO mode on M4 state
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_BUSY (0x0004) - The function is already active
SL_STATUS_INVALID_COUNT (0x002B) - Mismatch count
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_adc_set_channel_configuration#
sl_status_t sl_si91x_adc_set_channel_configuration (sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config)
Configure ADC channel parameters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_channel_config_t | [in] | adc_channel_config | : ADC channels configuration structure variable. |
| sl_adc_config_t | [in] | adc_config | : ADC operation configuration structure variable. |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_adc_register_event_callback#
sl_status_t sl_si91x_adc_register_event_callback (sl_adc_callback_t callback_event)
Register the user callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_callback_t | [in] | callback_event | Pointer to the function which needs to be called at the time of interrupt |
At the time of events, the function passed in the parameter is called with the respective event as the parameter. Before calling this function again, it is mandatory to call the sl_si91x_adc_unregister_event_callback function to unregister the callback, otherwise it returns SL_STATUS_BUSY error code.
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_BUSY (0x0004) - Driver is busy
sl_si91x_adc_unregister_event_callback#
void sl_si91x_adc_unregister_event_callback (void )
Un-register the user callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
It is mandatory to call this function before registering the callback again.
Pre-conditions:
Returns
none
sl_si91x_adc_configure_external_trigger#
sl_status_t sl_si91x_adc_configure_external_trigger (sl_adc_external_config_t adc_external_trigger)
Configure the ADC external trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_external_config_t | [in] | adc_external_trigger | : ADC external trigger configuration structure variable. |
Triggers can be used in PS4 State to collect the sample from a pre-defined channel. ADC can give a sample for the selected trigger with a trigger match. There are 3 external triggers, which are enabled by
ULPSS Timer interrupts
ULPSS GPIOs
M4SS Config_Timer. Trigger match can be checked by reading the sl_si91x_adc_get_external_trigger_status
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_configure_channel_sampling_rate#
sl_status_t sl_si91x_adc_configure_channel_sampling_rate (sl_adc_internal_config_t adc_internal_config, uint8_t channel_num)
Configure the ADC sampling rate for the ADC channels.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_internal_config_t | [in] | adc_internal_config | : Channel offset and frequency for each channel to set sampling rate. |
| uint8_t | [in] | channel_num | : Channel number |
It will set the channel offset value and channel frequency for each channel to set the sampling rate. The minimum allowed value is 3 to satisfy the Nyquist criteria of sampling rates. Freq_value 1 and 2 are not allowed.
Pre-conditions:
Pre-conditions:
Returns
sl_status_t : Returns 'SL_STATUS_OK' on successful execution.
sl_si91x_adc_get_external_trigger_status#
sl_status_t sl_si91x_adc_get_external_trigger_status (sl_adc_external_config_t adc_external_trigger, uint8_t * ext_trigger)
ADC can give a sample for the selected trigger with a trigger match.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_external_config_t | [in] | adc_external_trigger | : ADC external trigger configuration structure variable. |
| uint8_t * | [in] | ext_trigger | : The status of external trigger will be store in this. |
Read the ADC external trigger match.
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_clear_external_trigger#
sl_status_t sl_si91x_adc_clear_external_trigger (sl_adc_external_config_t adc_external_trigger)
Clear the ADC external trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_external_config_t | [in] | adc_external_trigger | : ADC external trigger configuration structure variable. |
After reading the trigger match can clear specific trigger using sl_si91x_adc_clear_external_trigger API.
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_configure_ping_pong_memory_address#
sl_status_t sl_si91x_adc_configure_ping_pong_memory_address (sl_adc_internal_config_t adc_internal_config, uint8_t channel_num)
Configure the ADC ping and pong memory location and length To configure the Ping and pong memory location along with length of ping memory and pong memory.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_internal_config_t | [in] | adc_internal_config | : ADC internal trigger configuration structure variable. |
| uint8_t | [in] | channel_num | : Channel number |
It is an applicable only for FIFO mode of ADC operation. FIFO mode supports dual buffer cyclic mode to avoid loss of data when buffer is full. In dual buffer cyclic mode, if Ping buffer is full for particular channel, incoming sampled data is written into Pong buffer such that, samples from Ping buffer are read back by controller during this time. That’s why there are two start addresses, two buffer lengths and two valid signals for each channel.
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_enable_ping_pong#
sl_status_t sl_si91x_adc_enable_ping_pong (uint8_t channel_num)
Enable ping pong for the corresponding ADC channels It is an applicable only for FIFO mode of ADC operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel_num | : Channel number |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_disable_ping_pong#
sl_status_t sl_si91x_adc_disable_ping_pong (uint8_t channel_num)
Disable ping pong for the corresponding ADC channels.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel_num | : Channel number |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_internal_per_channel_dma_enable#
sl_status_t sl_si91x_adc_internal_per_channel_dma_enable (uint8_t channel_num)
Enable DMA for the corresponding ADC channels.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel_num | : Channel number |
It is an applicable only for FIFO mode of ADC operation.
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_internal_per_channel_dma_disable#
sl_status_t sl_si91x_adc_internal_per_channel_dma_disable (uint8_t channel_num)
Disable DMA for the corresponding ADC channels.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel_num | : Channel number |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_configure_static_mode#
sl_status_t sl_si91x_adc_configure_static_mode (sl_adc_channel_config_t adc_channel_config, uint8_t channel_num)
Configure the ADC in Static Mode it can be programmed for setting input type, positive and negative input channel selection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_channel_config_t | [in] | adc_channel_config | : ADC channels configuration structure variable. |
| uint8_t | N/A | channel_num |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_adc_configure_fifo_mode#
sl_status_t sl_si91x_adc_configure_fifo_mode (sl_adc_channel_config_t adc_channel_config, uint8_t channel_num)
Configure the ADC in FIFO Mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_channel_config_t | [in] | adc_channel_config | : ADC channels configuration structure variable. |
| uint8_t | [in] | channel_num | : Channel number |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_adc_channel_enable#
sl_status_t sl_si91x_adc_channel_enable (uint8_t channel_num)
Enable the ADC channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel_num | : Channel number |
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_channel_disable#
sl_status_t sl_si91x_adc_channel_disable (uint8_t channel_num)
Disable the ADC channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel_num | : Channel number |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_set_power_mode#
sl_status_t sl_si91x_adc_set_power_mode (POWER_STATE state)
Set the Power On and off for ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| POWER_STATE | [in] | state | : ADC_POWER_ON - To powerup adc powergates, ADC_POWER_OFF - To powerdown adc powergates ( POWER_STATE ) |
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful,
SL_STATUS_OK (0x0000) - Success
sl_si91x_adc_set_noise_average_mode#
sl_status_t sl_si91x_adc_set_noise_average_mode (boolean_t state)
Enable or Disable the Noise averaging mode to ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| boolean_t | [in] | state | : 1 - To enable noise averaging mode, 0 - To disable noise averaging mode |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
Returns 'SL_STATUS_OK' on successful execution.
sl_si91x_adc_temperature_sensor_enable#
sl_status_t sl_si91x_adc_temperature_sensor_enable (void )
Enable BJT based Temperature sensor as an input to ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Operation mode of ADC should be Static.
Pre-conditions:
Pre-conditions:
Returns
Returns 'SL_STATUS_OK' on successful execution.
sl_si91x_adc_fifo_threshold_configuration#
sl_status_t sl_si91x_adc_fifo_threshold_configuration (sl_adc_config_t adc_config, sl_adc_fifo_thrld_config_t adc_fifo_threshold)
Configuring ADC fifo threshold.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_config_t | [in] | adc_config | : ADC operation configuration structure variable. |
| sl_adc_fifo_thrld_config_t | [in] | adc_fifo_threshold | : ADC fifo structure variable like an empty fifo, a full fifo threshold level. ( sl_adc_fifo_thrld_config_t ) |
Maximum FIFO depth is 16 can configure the threshold value.
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_adc_threshold_configuration#
sl_status_t sl_si91x_adc_threshold_configuration (sl_adc_threshold_config_t adc_threshold)
Configure the ADC threshold to compare threshold value with ADC data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_threshold_config_t | [in] | adc_threshold | : ADC threshold configuration structure variables. |
This is valid in ADC Static mode only.
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
Returns 'SL_STATUS_OK' on successful execution.
sl_si91x_adc_read_data#
sl_status_t sl_si91x_adc_read_data (sl_adc_channel_config_t adcchconfig, uint8_t channel_num)
Read the ADC samples when FIFO mode is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_channel_config_t | [in] | adcchconfig | : ADC channels configuration structure variable. |
| uint8_t | [in] | channel_num | channel_num : Channel number |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_adc_read_data_static#
sl_status_t sl_si91x_adc_read_data_static (sl_adc_channel_config_t adc_channel_config, sl_adc_config_t adc_config, uint16_t * adc_value)
Read the ADC samples when static mode is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_channel_config_t | [in] | adc_channel_config | : ADC channels configuration structure variable. |
| sl_adc_config_t | [in] | adc_config | : ADC operation configuration structure variable. |
| uint16_t * | [in] | adc_value | : Store the reading data on adc_value. |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Mismatch Range
sl_si91x_adc_get_sampling_rate#
uint32_t sl_si91x_adc_get_sampling_rate (uint8_t channel_num)
To get the channel sampling rate value which is configured to ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel_num | : Channel number |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
Returns sampling rate what it get from register
sl_si91x_adc_deinit#
sl_status_t sl_si91x_adc_deinit (sl_adc_config_t adc_config)
Uninitialize the ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_config_t | [in] | adc_config | : ADC operation configuration structure variable. |
If the DMA is enabled, it also uninitializes the DMA.
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_start#
sl_status_t sl_si91x_adc_start (sl_adc_config_t adc_config)
Start the ADC operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_config_t | [in] | adc_config | : ADC operation configuration structure variable. |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_stop#
sl_status_t sl_si91x_adc_stop (sl_adc_config_t adc_config)
Stop the ADC operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_adc_config_t | [in] | adc_config | : ADC operation configuration structure variable. |
Pre-conditions:
Pre-conditions:
Pre-conditions:
Pre-conditions:
Returns
status 0 if successful, else error code as follow
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
sl_si91x_adc_get_version#
sl_adc_version_t sl_si91x_adc_get_version (void )
Get the ADC version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
It returns the API version of ADC.
Returns
(sl_adc_version_t) type structure