USART#

Modules#

sl_si91x_usart_control_config_t

sl_usart_version_t

Enumerations#

enum
SL_USART_EVENT_SEND_COMPLETE = ARM_USART_EVENT_SEND_COMPLETE
SL_USART_EVENT_RECEIVE_COMPLETE = ARM_USART_EVENT_RECEIVE_COMPLETE
SL_USART_EVENT_TRANSFER_COMPLETE = ARM_USART_EVENT_TRANSFER_COMPLETE
SL_USART_EVENT_TX_COMPLETE = ARM_USART_EVENT_TX_COMPLETE
SL_USART_EVENT_TX_UNDERFLOW = ARM_USART_EVENT_TX_UNDERFLOW
SL_USART_EVENT_RX_OVERFLOW = ARM_USART_EVENT_RX_OVERFLOW
SL_USART_EVENT_RX_TIMEOUT = ARM_USART_EVENT_RX_TIMEOUT
SL_USART_EVENT_RX_BREAK = ARM_USART_EVENT_RX_BREAK
SL_USART_EVENT_RX_FRAMING_ERROR = ARM_USART_EVENT_RX_FRAMING_ERROR
SL_USART_EVENT_RX_PARITY_ERROR = ARM_USART_EVENT_RX_PARITY_ERROR
SL_USART_EVENT_CTS = ARM_USART_EVENT_CTS
SL_USART_EVENT_DSR = ARM_USART_EVENT_DSR
SL_USART_EVENT_DCD = ARM_USART_EVENT_DCD
SL_USART_EVENT_RI = ARM_USART_EVENT_RI
}

USART/UART Events.

enum
SL_POWER_OFF = ARM_POWER_OFF
SL_POWER_LOW = ARM_POWER_LOW
SL_POWER_FULL = ARM_POWER_FULL
SL_POWER_MODE_LAST
}

General power states.

enum
SL_USART_DATA_BITS_5 = ARM_USART_DATA_BITS_5
SL_USART_DATA_BITS_6 = ARM_USART_DATA_BITS_6
SL_USART_DATA_BITS_7 = ARM_USART_DATA_BITS_7
SL_USART_DATA_BITS_8 = ARM_USART_DATA_BITS_8
SL_USART_DATA_BITS_9 = ARM_USART_DATA_BITS_9
}

Databit selection.

enum
SL_USART_NO_PARITY = ARM_USART_PARITY_NONE
SL_USART_EVEN_PARITY = ARM_USART_PARITY_EVEN
SL_USART_ODD_PARITY = ARM_USART_PARITY_ODD
}

Parity selection.

enum
SL_USART_RTS_CLEAR = ARM_USART_RTS_CLEAR
SL_USART_RTS_SET = ARM_USART_RTS_SET
SL_USART_DTR_CLEAR = ARM_USART_DTR_CLEAR
SL_USART_DTR_SET = ARM_USART_DTR_SET
SL_USART_MODEM_CONTROL_LAST
}

USART Modem control selection.

enum
SL_USART_STOP_BITS_1 = ARM_USART_STOP_BITS_1
SL_USART_STOP_BITS_1_5 = ARM_USART_STOP_BITS_1_5
SL_USART_STOP_BITS_2 = ARM_USART_STOP_BITS_2
}

Stop bits selection, used for asynchronous operation.

enum
SL_USART_FLOW_CONTROL_NONE = ARM_USART_FLOW_CONTROL_NONE
SL_USART_FLOW_CONTROL_CTS = ARM_USART_FLOW_CONTROL_CTS
SL_USART_FLOW_CONTROL_RTS = ARM_USART_FLOW_CONTROL_RTS
SL_USART_FLOW_CONTROL_RTS_CTS = ARM_USART_FLOW_CONTROL_RTS_CTS
}

Hardware Flow Control Selection.

enum
SL_USART_MODE_ASYNCHRONOUS = ARM_USART_MODE_ASYNCHRONOUS
SL_USART_MODE_SYNCHRONOUS_MASTER = ARM_USART_MODE_SYNCHRONOUS_MASTER
SL_USART_MODE_SYNCHRONOUS_SLAVE = ARM_USART_MODE_SYNCHRONOUS_SLAVE
SL_USART_MODE_SINGLE_WIRE = ARM_USART_MODE_SINGLE_WIRE
SL_USART_MODE_IRDA = ARM_USART_MODE_IRDA
}

USART Mode selection.

enum
SL_USART_MISC_CONTROL_NONE
SL_USART_SET_DEFAULT_TX_VALUE = ARM_USART_SET_DEFAULT_TX_VALUE
SL_USART_CONTROL_TX = ARM_USART_CONTROL_TX
SL_USART_CONTROL_RX = ARM_USART_CONTROL_RX
SL_USART_CONTROL_BREAK = ARM_USART_CONTROL_BREAK
SL_USART_ABORT_SEND = ARM_USART_ABORT_SEND
SL_USART_ABORT_RECEIVE = ARM_USART_ABORT_RECEIVE
SL_USART_ABORT_TRANSFER = ARM_USART_ABORT_TRANSFER
}

USART misc control selection.

Typedefs#

typedef ARM_USART_SignalEvent_t
typedef ARM_USART_STATUS
typedef ARM_POWER_STATE
typedef ARM_USART_MODEM_CONTROL
typedef ARM_USART_MODEM_STATUS
typedef ARM_USART_CAPABILITIES
typedef ARM_DRIVER_USART
typedef USART_RESOURCES
typedef const void *

Functions#

sl_status_t
sl_si91x_usart_init(usart_peripheral_t usart_instance, sl_usart_handle_t *usart_handle)

Initilize the USART/UART module.

sl_status_t
sl_si91x_usart_deinit(sl_usart_handle_t usart_handle)

Uninitialize the USART/UART module.

sl_status_t
sl_si91x_usart_register_event_callback(sl_usart_signal_event_t callback_event)

Register the user callback function.

void

Unregister the user callback function.

sl_status_t
sl_si91x_usart_multiple_instance_register_event_callback(usart_peripheral_t usart_instance, sl_usart_signal_event_t callback_event)

This function registers the user callback function for multiple usart instances i.e., to use different instance (USART_O, UART_1, ULP_UART) this API need to use.

void

Unregister the user callback function in case of multiple usart insatances.

sl_status_t
sl_si91x_usart_send_data(sl_usart_handle_t usart_handle, const void *data, uint32_t data_length)

Send the USART data when USART/UART is configured.

sl_status_t
sl_si91x_usart_async_send_data(sl_usart_handle_t usart_handle, const void *data, uint32_t data_length)

To Send the data in async mode when USART/UART is configured.

sl_status_t
sl_si91x_usart_receive_data(sl_usart_handle_t usart_handle, void *data, uint32_t data_length)

To receive the data when USART/UART is configured.

sl_status_t
sl_si91x_usart_async_receive_data(sl_usart_handle_t usart_handle, void *data, uint32_t data_length)

To receive the data in async mode when USART/UART is configured.

sl_status_t
sl_si91x_usart_transfer_data(sl_usart_handle_t usart_handle, const void *data_out, void *data_in, uint32_t data_length)

To send and receive the data when USART in Synchronous mode is enabled.

uint32_t
sl_si91x_usart_get_tx_data_count(sl_usart_handle_t usart_handle)

To get the TX data count of USART/UART This function will return the USART data transferred count.

uint32_t
sl_si91x_usart_get_rx_data_count(sl_usart_handle_t usart_handle)

To get the RX data count of USART/UART This function will return the USART/UART data received count.

sl_status_t
sl_si91x_usart_set_configuration(sl_usart_handle_t usart_handle, sl_si91x_usart_control_config_t *control_configuration)

To control and configure the USART/UART module in different configurations.

sl_status_t
sli_si91x_usart_set_non_uc_configuration(sl_usart_handle_t usart_handle, sl_si91x_usart_control_config_t *control_configuration)
sl_usart_status_t
sl_si91x_usart_get_status(sl_usart_handle_t usart_handle)

To get the USART/UART status.

sl_status_t
sl_si91x_usart_set_modem_control(sl_usart_handle_t usart_handle, sl_usart_modem_control_t control)

This function will set the USART modem control line.

sl_usart_modem_status_t
sl_si91x_usart_get_modem_status(sl_usart_handle_t usart_handle)

This function return USART modem control status.

This function is used to know the USART version.

sl_status_t
sl_si91x_usart_get_configurations(uint8_t usart_module, sl_si91x_usart_control_config_t *usart_config)

Get the USART configurations set in the module such as baudrate, parity bit stop bits etc.

Enumeration Documentation#

usart_event_typedef_t#

usart_event_typedef_t

USART/UART Events.

Enumerator
SL_USART_EVENT_SEND_COMPLETE

Send complete event.

SL_USART_EVENT_RECEIVE_COMPLETE

Receive complete event.

SL_USART_EVENT_TRANSFER_COMPLETE

Transfer complete event.

SL_USART_EVENT_TX_COMPLETE

Tx complete event event.

SL_USART_EVENT_TX_UNDERFLOW

TX underflow event.

SL_USART_EVENT_RX_OVERFLOW

RX overflow event.

SL_USART_EVENT_RX_TIMEOUT

RX timeout event.

SL_USART_EVENT_RX_BREAK

RX break event.

SL_USART_EVENT_RX_FRAMING_ERROR

RX Framing error event.

SL_USART_EVENT_RX_PARITY_ERROR

RX parity error event.

SL_USART_EVENT_CTS

CTS event.

SL_USART_EVENT_DSR

DSR EVENT.

SL_USART_EVENT_DCD

DCD event.

SL_USART_EVENT_RI

RI Event.


power_mode_typedef_t#

power_mode_typedef_t

General power states.

Enumerator
SL_POWER_OFF

Power Off.

SL_POWER_LOW

Power low.

SL_POWER_FULL

Power Full.

SL_POWER_MODE_LAST

usart_databits_typedef_t#

usart_databits_typedef_t

Databit selection.

Enumerator
SL_USART_DATA_BITS_5

5 data bits

SL_USART_DATA_BITS_6

6 data bits

SL_USART_DATA_BITS_7

7 data bits

SL_USART_DATA_BITS_8

8 data bits

SL_USART_DATA_BITS_9

9 data bits


usart_parity_typedef_t#

usart_parity_typedef_t

Parity selection.

Enumerator
SL_USART_NO_PARITY

No parity.

SL_USART_EVEN_PARITY

Even parity.

SL_USART_ODD_PARITY

Odd parity.


usart_modem_control_typedef_t#

usart_modem_control_typedef_t

USART Modem control selection.

Enumerator
SL_USART_RTS_CLEAR

RTS clear.

SL_USART_RTS_SET

RTS Set.

SL_USART_DTR_CLEAR

DTR Clear.

SL_USART_DTR_SET

Activate DTR.

SL_USART_MODEM_CONTROL_LAST

usart_stopbit_typedef_t#

usart_stopbit_typedef_t

Stop bits selection, used for asynchronous operation.

Enumerator
SL_USART_STOP_BITS_1

1 stop bits.

SL_USART_STOP_BITS_1_5

1.5 stop bits.

SL_USART_STOP_BITS_2

2 stop bits


usart_hwflowcontol_typedef_t#

usart_hwflowcontol_typedef_t

Hardware Flow Control Selection.

Enumerator
SL_USART_FLOW_CONTROL_NONE

No hardware flow control.

SL_USART_FLOW_CONTROL_CTS

CTS signal is enabled for TX flow control.

SL_USART_FLOW_CONTROL_RTS

RTS signal is enabled for RX flow control.

SL_USART_FLOW_CONTROL_RTS_CTS

CTS and RTS signals are enabled for TX and RX flow control.


usart_mode_typedef_t#

usart_mode_typedef_t

USART Mode selection.

Enumerator
SL_USART_MODE_ASYNCHRONOUS

Asynchronous mode.

SL_USART_MODE_SYNCHRONOUS_MASTER

Synchronous mode master.

SL_USART_MODE_SYNCHRONOUS_SLAVE

Synchronous mode slave.

SL_USART_MODE_SINGLE_WIRE

UART Single-wire (half-duplex); arg = Baudrate.

SL_USART_MODE_IRDA

UART IrDA; arg = Baudrate.


usart_misc_control_typedef_t#

usart_misc_control_typedef_t

USART misc control selection.

Enumerator
SL_USART_MISC_CONTROL_NONE
SL_USART_SET_DEFAULT_TX_VALUE

Set default TX value.

SL_USART_CONTROL_TX

Set transfer line.

SL_USART_CONTROL_RX

Set receive line.

SL_USART_CONTROL_BREAK

Set USART control break.

SL_USART_ABORT_SEND

Abort send.

SL_USART_ABORT_RECEIVE

Abort receive.

SL_USART_ABORT_TRANSFER

Abort transfer.


Typedef Documentation#

sl_usart_signal_event_t#

typedef ARM_USART_SignalEvent_t sl_usart_signal_event_t

sl_usart_status_t#

typedef ARM_USART_STATUS sl_usart_status_t

sl_usart_power_state_t#

typedef ARM_POWER_STATE sl_usart_power_state_t

sl_usart_modem_control_t#

typedef ARM_USART_MODEM_CONTROL sl_usart_modem_control_t

sl_usart_modem_status_t#

typedef ARM_USART_MODEM_STATUS sl_usart_modem_status_t

sl_usart_capabilities_t#

typedef ARM_USART_CAPABILITIES sl_usart_capabilities_t

sl_usart_driver_t#

typedef ARM_DRIVER_USART sl_usart_driver_t

usart_resources_t#

typedef USART_RESOURCES usart_resources_t

sl_usart_handle_t#

typedef const void* sl_usart_handle_t

Function Documentation#

sl_si91x_usart_init#

sl_status_t sl_si91x_usart_init (usart_peripheral_t usart_instance, sl_usart_handle_t * usart_handle)

Initilize the USART/UART module.

Parameters
TypeDirectionArgument NameDescription
usart_peripheral_t[in]usart_instance

Pointer to the USART/UART driver

sl_usart_handle_t *[in]usart_handle

Callback function which needs to be called on data transfer

This function will configure the clocks for USART/UART module and also initialization of the DMA for UART/USART, if DMA is enabled for data transfers.

This function will configure the clocks for USART/UART module and also initialize the DMA for UART/USART if DMA is enabled for data transfers.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_FAIL (0x0001) - Fail, UART/USART initialization failed

    • SL_STATUS_OK (0x0000) - Success, UART/USART initialization done properly


sl_si91x_usart_deinit#

sl_status_t sl_si91x_usart_deinit (sl_usart_handle_t usart_handle)

Uninitialize the USART/UART module.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

This function will disable the clocks for USART/UART module and also Deinit the DMA for UART/USART if DMA is enabled for data transfers.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_FAIL (0x0001) - Fail, UART/USART Deinitialization failed

    • SL_STATUS_OK (0x0000) - Success, UART/USART Deinitialization done properly


sl_si91x_usart_register_event_callback#

sl_status_t sl_si91x_usart_register_event_callback (sl_usart_signal_event_t callback_event)

Register the user callback function.

Parameters
TypeDirectionArgument NameDescription
sl_usart_signal_event_t[in]callback_event

Pointer to the function which needs to be called at the time of interrupt

If another callback is registered without unregistering previous callback then, it returns an error code, so it is mandatory to unregister the callback before registering to another callback.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_usart_unregister_event_callback#

void sl_si91x_usart_unregister_event_callback (void )

Unregister the user callback function.

Parameters
TypeDirectionArgument NameDescription
void[in]

Unregister the user callback function before regsitering new callback function.

Returns

  • none


sl_si91x_usart_multiple_instance_register_event_callback#

sl_status_t sl_si91x_usart_multiple_instance_register_event_callback (usart_peripheral_t usart_instance, sl_usart_signal_event_t callback_event)

This function registers the user callback function for multiple usart instances i.e., to use different instance (USART_O, UART_1, ULP_UART) this API need to use.

Parameters
TypeDirectionArgument NameDescription
usart_peripheral_t[in]usart_instance

Usart Instance

sl_usart_signal_event_t[in]callback_event

Pointer to the function which needs to be called at the time of interrupt

Returns

  • status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_usart_multiple_instance_unregister_event_callback#

void sl_si91x_usart_multiple_instance_unregister_event_callback (usart_peripheral_t usart_instance)

Unregister the user callback function in case of multiple usart insatances.

Parameters
TypeDirectionArgument NameDescription
usart_peripheral_t[in]usart_instance

Usart Instance

Returns

  • none


sl_si91x_usart_send_data#

sl_status_t sl_si91x_usart_send_data (sl_usart_handle_t usart_handle, const void * data, uint32_t data_length)

Send the USART data when USART/UART is configured.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

const void *[in]data

Pointer to the variable which contains transfer data

uint32_t[in]data_length

Data_length to Send

if DMA mode is set this function will configure the DMA channel and enables the DMA channel , then transfer's the data pointed to it else it fill the data to the transfer FIFO and transfer the data

Returns

  • status 0 if successful, else error code SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is invalid argument SL_STATUS_FAIL (0x0001) - Fail , Data transfer failed SL_STATUS_BUSY (0x0004) - Busy ,already data transfer is going on SL_STATUS _OK (0X000) - Success ,UART/USART initialization done properly


sl_si91x_usart_async_send_data#

sl_status_t sl_si91x_usart_async_send_data (sl_usart_handle_t usart_handle, const void * data, uint32_t data_length)

To Send the data in async mode when USART/UART is configured.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

const void *[in]data

Pointer to the variable which will store the transferred data

uint32_t[in]data_length

Data_length to transfer

This function returns immediately(non blocking) and data transfer happens asyncronously. Once the data transfer compeletes , registered user callback get invoked

Returns

  • status 0 if successful, else error code SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is invalid argument SL_STATUS_FAIL (0x0001) - Fail , Data transfer failed SL_STATUS_BUSY (0x0004) - Busy ,already data transfer is going on SL_STATUS _OK (0X000) - Success ,UART/USART initialization done properly


sl_si91x_usart_receive_data#

sl_status_t sl_si91x_usart_receive_data (sl_usart_handle_t usart_handle, void * data, uint32_t data_length)

To receive the data when USART/UART is configured.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

void *[in]data

Pointer to the variable which will store the received data

uint32_t[in]data_length

Data_length to receive

If DMA mode is set, it configures the DMA channel, enables the DMA channel, and receives data via DMA. If DMA mode is not set, it receives the data from FIFO.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_FAIL (0x0001) - Fail, Data transfer failed

    • SL_STATUS_BUSY (0x0004) - Busy, already data transfer is going on

    • SL_STATUS_OK (0x0000) - Success, UART/USART initialization done properly


sl_si91x_usart_async_receive_data#

sl_status_t sl_si91x_usart_async_receive_data (sl_usart_handle_t usart_handle, void * data, uint32_t data_length)

To receive the data in async mode when USART/UART is configured.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

void *[in]data

Pointer to the variable which will store the received data

uint32_t[in]data_length

Data_length to receive

This function returns immediately(Non blocking) and data reception happens asyncronously. Once the data reception compeletes, registered user callback get invoked

Returns

  • status 0 if successful, else error code SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is invalid argument SL_STATUS_FAIL (0x0001) - Fail , Data transfer failed SL_STATUS_BUSY (0x0004) - Busy ,already data transfer is going on SL_STATUS _OK (0X000) - Success ,UART/USART initialization done properly


sl_si91x_usart_transfer_data#

sl_status_t sl_si91x_usart_transfer_data (sl_usart_handle_t usart_handle, const void * data_out, void * data_in, uint32_t data_length)

To send and receive the data when USART in Synchronous mode is enabled.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

const void *[in]data_out

Pointer to the variable which will store the data to be transferred

void *[in]data_in

Pointer to the variable which will store the received data

uint32_t[in]data_length

Data_length to receive

This function sends and receives the data to and from usart transmitter and receiver in synchronous mode of operation. Configure the DMA channel and enables the DMA channel, if DMA mode is set and transfer's the data pointed to it else transfer the data from fifo.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument

    • SL_STATUS_FAIL (0x0001) - Fail, Data transfer failed

    • SL_STATUS_BUSY (0x0004) - Busy, already data transfer is going on

    • SL_STATUS_OK (0x0000) - Success, UART/USART initialization done properly

Note


sl_si91x_usart_get_tx_data_count#

uint32_t sl_si91x_usart_get_tx_data_count (sl_usart_handle_t usart_handle)

To get the TX data count of USART/UART This function will return the USART data transferred count.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

Returns

  • return the no of bytes transferred


sl_si91x_usart_get_rx_data_count#

uint32_t sl_si91x_usart_get_rx_data_count (sl_usart_handle_t usart_handle)

To get the RX data count of USART/UART This function will return the USART/UART data received count.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

Returns

  • return the no of bytes received


sl_si91x_usart_set_configuration#

sl_status_t sl_si91x_usart_set_configuration (sl_usart_handle_t usart_handle, sl_si91x_usart_control_config_t * control_configuration)

To control and configure the USART/UART module in different configurations.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

sl_si91x_usart_control_config_t *[in]control_configuration

pointer to the USART configurations

This function configure the USART in different configurations such as USART mode, Data Bits, Parity , stop bits, flow control and baud rate.

Returns

  • status 0 if successful, else error code

    • SL_STATUS_BUSY (0x0004) - Busy ,already data transfer is going on

    • SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is invalid argument

    • SL_STATUS_INVALID_MODE (0x0024) - USART Invalid mode of operation

    • SL_STATUS_NOT_SUPPORTED(0x000F) - Feature not supported

    • SL_STATUS _OK (0X000) - Success ,UART/USART initialization done properly


sli_si91x_usart_set_non_uc_configuration#

sl_status_t sli_si91x_usart_set_non_uc_configuration (sl_usart_handle_t usart_handle, sl_si91x_usart_control_config_t * control_configuration)
Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_tN/Ausart_handle
sl_si91x_usart_control_config_t *N/Acontrol_configuration

sl_si91x_usart_get_status#

sl_usart_status_t sl_si91x_usart_get_status (sl_usart_handle_t usart_handle)

To get the USART/UART status.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

This function will return USART/UART transfer and receive status

Returns

  • usart line status tx busy ,rx_busy, tx_underflow ,rx overflow, rx break, rx framing error rx parity error


sl_si91x_usart_set_modem_control#

sl_status_t sl_si91x_usart_set_modem_control (sl_usart_handle_t usart_handle, sl_usart_modem_control_t control)

This function will set the USART modem control line.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

sl_usart_modem_control_t[in]control

usart modem control

Returns

  • status 0 if successful, else error code

    • SL_STATUS_NOT_SUPPORTED(0x000F) - Feature not supported

    • SL_STATUS _OK (0x000) - Success ,UART/USART initialization done properly


sl_si91x_usart_get_modem_status#

sl_usart_modem_status_t sl_si91x_usart_get_modem_status (sl_usart_handle_t usart_handle)

This function return USART modem control status.

Parameters
TypeDirectionArgument NameDescription
sl_usart_handle_t[in]usart_handle

Pointer to the USART/UART driver

Returns

  • usart modem status states are active or not


sl_si91x_usart_get_version#

sl_usart_version_t sl_si91x_usart_get_version (void )

This function is used to know the USART version.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns


sl_si91x_usart_get_configurations#

sl_status_t sl_si91x_usart_get_configurations (uint8_t usart_module, sl_si91x_usart_control_config_t * usart_config)

Get the USART configurations set in the module such as baudrate, parity bit stop bits etc.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]usart_module

USART peripheral type

  • 0 - USART0

  • 1 - UART1

  • 2 - ULP_UART

sl_si91x_usart_control_config_t *[in]usart_config

Pointer to the USART configurations structure

Returns

  • status 0 if successful, else error code

    • SL_STATUS_NULL_POINTER(0x0022) - Invalid NULL pointer received as argument \

    • SL_STATUS _OK (0x000) - Success ,UART/USART configurations retrieved successfully \