RO Temperature Sensor#
Enumerations#
RO temperature sensor reference clock.
Enable/Disable RO temperature sensor.
Enable/Disable BJT based temperature update.
Enable/Disable RO periodic temperature checking.
RO temperature periodic check time.
Functions#
Set reference clock count for RO temperature sensor.
Select reference clock for RO temperature sensor.
Enable/disable RO temperature sensor.
Set nominal value for RO temperature sensor.
Read value from RO temperature sensor.
Calculate temperature from RO temperature sensor reading.
Update temperature for RO temperature sensor.
Get reference clock count for RO temperature sensor.
Get ptat clock count for RO temperature sensor.
Update temperature periodically for RO temperature sensor.
Enumeration Documentation#
sl_ro_reference_clock_t#
sl_ro_reference_clock_t
RO temperature sensor reference clock.
| Enumerator | |
|---|---|
| SL_RO_REF_CLK | Enable RO kHz clock from analog as reference clock. |
| SL_RO_FSM_CLK | Enable MCU FSM clock as reference clock. |
| SL_RO_CLK_LAST | Last member of enum for validation. |
sl_ro_temperature_state_t#
sl_ro_temperature_state_t
Enable/Disable RO temperature sensor.
| Enumerator | |
|---|---|
| SL_RO_TEMPERATURE_DISABLE | Temperature sensing disable. |
| SL_RO_TEMPERATURE_ENABLE | Temperature sensing enable. |
| SL_RO_TEMPERATURE_LAST | Last member of enum for validation. |
sl_ro_temperature_update_t#
sl_ro_temperature_update_t
Enable/Disable BJT based temperature update.
| Enumerator | |
|---|---|
| SL_RO_TEMP_BJT_UPDATE_ENABLE | Enable BJT based temperature through RO calculation. |
| SL_RO_TEMP_SPI_UPDATE_ENABLE | Disable BJT based temperature through RO calculation and Enable update through SPI. |
| SL_RO_TEMP_BJT_UPDATE_LAST | Last member of enum for validation. |
sl_ro_temperature_periodic_check_t#
sl_ro_temperature_periodic_check_t
Enable/Disable RO periodic temperature checking.
| Enumerator | |
|---|---|
| SL_RO_TEMPERATURE_PERIODIC_DISABLE | Periodic temperature checking disable. |
| SL_RO_TEMPERATURE_PERIODIC_ENABLE | Periodic temperature checking enable. |
| SL_RO_TEMPERATURE_PERIODIC_LAST | Last member of enum for validation. |
sl_ro_temperature_trigger_time_t#
sl_ro_temperature_trigger_time_t
RO temperature periodic check time.
| Enumerator | |
|---|---|
| SL_RO_TEMPERATURE_TRIGGER_1SEC | RO temperature update for every 1second. |
| SL_RO_TEMPERATURE_TRIGGER_2SEC | RO temperature update for every 2seconds. |
| SL_RO_TEMPERATURE_TRIGGER_4SEC | RO temperature update for every 4seconds. |
| SL_RO_TEMPERATURE_TRIGGER_5SEC | RO temperature update for every 5seconds. |
| SL_RO_TEMPERATURE_TRIGGER_LAST | Last member of enum for validation. |
Function Documentation#
sl_si91x_ro_temperature_set_count#
sl_status_t sl_si91x_ro_temperature_set_count (uint32_t count)
Set reference clock count for RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | count | Count of reference clock on which ptat clock counts |
This API is used to set the count of reference clock on which ptat clock counts.
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_INVALID_PARAMETER (0x0021) , The parameter is invalid argument
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_select_reference_clock#
sl_status_t sl_si91x_ro_temperature_select_reference_clock (sl_ro_reference_clock_t ref_clk)
Select reference clock for RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ro_reference_clock_t | [in] | ref_clk | Reference clock selection:
|
This API is used to select the reference clock to the temperature sensor
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_INVALID_PARAMETER (0x0021) , The parameter is invalid argument
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_enable#
sl_status_t sl_si91x_ro_temperature_enable (sl_ro_temperature_state_t state)
Enable/disable RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ro_temperature_state_t | [in] | state | Enable / disable the temperature sensor:
|
This API is used to enable / disable the temperature sensor
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_INVALID_PARAMETER (0x0021) , The parameter is invalid argument
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_nominal#
sl_status_t sl_si91x_ro_temperature_nominal (uint32_t value)
Set nominal value for RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | value | Calibrated temperature value |
This API is used to set the nominal value of the temperature sensor
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_INVALID_PARAMETER (0x0021) , The parameter is invalid argument
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_read#
sl_status_t sl_si91x_ro_temperature_read (int32_t * temperature)
Read value from RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t * | [out] | temperature | Temperature value reading |
This API is used to read the temperature value
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_based_update#
sl_status_t sl_si91x_ro_temperature_based_update (sl_ro_temperature_update_t enable)
Calculate temperature from RO temperature sensor reading.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ro_temperature_update_t | [in] | enable | Enable RO based BJT temperature update |
This API is used to updating temperature through RO based calculation
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_INVALID_PARAMETER (0x0021) , The parameter is invalid argument
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_load#
sl_status_t sl_si91x_ro_temperature_load (uint8_t temperature)
Update temperature for RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | temperature | Known temperature |
This API is used to updating temperature
Returns
SL_STATUS_OK on success
sl_si91x_ro_temperature_get_reference_clk_count#
sl_status_t sl_si91x_ro_temperature_get_reference_clk_count (uint32_t * ref_count)
Get reference clock count for RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [out] | ref_count | Count of f1 clock cycles |
This API is used to read the reference clock count
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_get_ptat_clk_count#
sl_status_t sl_si91x_ro_temperature_get_ptat_clk_count (uint32_t * ptat_count)
Get ptat clock count for RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [out] | ptat_count | Count of f2 clock cycles |
This API is used to read the ptat clock count
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer
sl_si91x_ro_temperature_periodic_update#
sl_status_t sl_si91x_ro_temperature_periodic_update (sl_ro_temperature_periodic_check_t periodic_check, sl_ro_temperature_trigger_time_t trigger_time)
Update temperature periodically for RO temperature sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ro_temperature_periodic_check_t | [in] | periodic_check | Enable periodic checking of temperature |
| sl_ro_temperature_trigger_time_t | [in] | trigger_time | Periodic check time in sec:
|
This API is used to update the temperature periodically after some time
Returns
Status 0 if successful, else error code:
SL_STATUS_OK on success
SL_STATUS_INVALID_PARAMETER (0x0021) , The parameter is invalid argument
SL_STATUS_NULL_POINTER (0x0022) , The parameter is null pointer