Synchronous Serial Interface#

Modules#

sl_ssi_version_t

sl_ssi_control_config_t

sl_ssi_clock_config_t

Enumerations#

enum
SSI_EVENT_TRANSFER_COMPLETE = ARM_SPI_EVENT_TRANSFER_COMPLETE
SSI_EVENT_DATA_LOST = ARM_SPI_EVENT_DATA_LOST
SSI_EVENT_MODE_FAULT = ARM_SPI_EVENT_MODE_FAULT
}

Enumeration for different SSI callback events.

enum
SL_SSI_PERIPHERAL_CPOL0_CPHA0 = ARM_SPI_CPOL0_CPHA0
SL_SSI_PERIPHERAL_CPOL0_CPHA1 = ARM_SPI_CPOL0_CPHA1
SL_SSI_PERIPHERAL_CPOL1_CPHA0 = ARM_SPI_CPOL1_CPHA0
SL_SSI_PERIPHERAL_CPOL1_CPHA1 = ARM_SPI_CPOL1_CPHA1
SL_SSI_PERIPHERAL_TI_SSI = ARM_SPI_TI_SSI
SL_SSI_PERIPHERAL_MICROWIRE = ARM_SPI_MICROWIRE
SL_SSI_PERIPHERAL_MODE_LAST
}

Enumeration for different SSI peripheral clock modes.

enum
SL_SSI_MASTER_ACTIVE = ARM_SPI_MODE_MASTER
SL_SSI_SLAVE_ACTIVE = ARM_SPI_MODE_SLAVE
SL_SSI_ULP_MASTER_ACTIVE
SL_SSI_INSTANCE_LAST
}

Enumeration for different SSI peripheral device modes.

enum
SSI_SLAVE_0
SSI_SLAVE_1
SSI_SLAVE_2
SSI_SLAVE_3
SSI_SLAVE_NUMBER_LAST_ENUM
}

Enumeration for SSI Secondary numbers.

Typedefs#

typedef ARM_POWER_STATE

renaming arm power state structure

typedef ARM_SPI_STATUS

renaming arm SPI status

typedef ARM_DRIVER_SPI

Renaming SSI driver structure.

typedef const void *

SSI Handle to be passed into APIs.

typedef ARM_SPI_SignalEvent_t

Callback typedef for SSI.

Variables#

uint8_t

Release version number.

uint8_t

SQA version number.

uint8_t

DEV version number.

uint8_t

bit width either 8 or 16 bit

uint32_t

mode such as Master or Slave mode

uint32_t

clock mode such as CPOL0 CPHA1

uint32_t

baud rate for SSI

uint32_t

Delay for receive input signal.

uint16_t

Clock Division Factor.

uint16_t

intf PLL control value

uint32_t

intf PLL clock frequency

uint32_t

intf PLL reference clock frequency

uint32_t

SoC PLL Clock frequency.

uint32_t

SoC PLL reference clock frequency.

uint8_t

SoC PLL count value.

Functions#

sl_status_t
sl_si91x_ssi_configure_clock(sl_ssi_clock_config_t *clock_config)

Set the clock for the SSI peripheral, Configures the PLL clock and SOC clock with the value set by user in the clock configuration structure.

sl_status_t
sl_si91x_ssi_init(sl_ssi_instance_t instance, sl_ssi_handle_t *ssi_handle)

Initialize the SSI.

sl_status_t
sl_si91x_ssi_deinit(sl_ssi_handle_t ssi_handle)

Uninitialize the SSI.

sl_status_t
sl_si91x_ssi_set_configuration(sl_ssi_handle_t ssi_handle, sl_ssi_control_config_t *control_configuration, sl_ssi_slave_number_t slave_number)

Control and configure the SSI.

sl_status_t
sl_si91x_ssi_receive_data(sl_ssi_handle_t ssi_handle, void *data, uint32_t data_length)

Start receiving the data from the SSI interface.

sl_status_t
sl_si91x_ssi_send_data(sl_ssi_handle_t ssi_handle, const void *data, uint32_t data_length)

Start sending the data from the SSI interface.

sl_status_t
sl_si91x_ssi_transfer_data(sl_ssi_handle_t ssi_handle, const void *data_out, void *data_in, uint32_t data_length)

Start to send and receive bi-directional full duplex data to/from the SPI secondary.

sl_si91x_ssi_get_status(sl_ssi_handle_t ssi_handle)

Get the SSI status.

Get the SSI version.

uint32_t
sl_si91x_ssi_get_rx_data_count(sl_ssi_handle_t ssi_handle)

Get data receive count of the SSI.

uint32_t
sl_si91x_ssi_get_tx_data_count(sl_ssi_handle_t ssi_handle)

Get the transmit data count of SSI.

sl_status_t
sl_si91x_ssi_register_event_callback(sl_ssi_handle_t ssi_handle, sl_ssi_signal_event_t callback_event)

Register the user event callback.

void

Unregister the user event callback.

uint32_t
sl_si91x_ssi_get_clock_division_factor(sl_ssi_handle_t ssi_handle)

Fetch the clock division factor.

uint32_t
sl_si91x_ssi_get_frame_length(sl_ssi_handle_t ssi_handle)

Fetch the frame length i.e., bit width.

uint32_t
sl_si91x_ssi_get_tx_fifo_threshold(sl_ssi_handle_t ssi_handle)

To fetch the transmit FIFO threshold value, this value controls the level of entries at which the transmit FIFO controller triggers an interrupt.

uint32_t
sl_si91x_ssi_get_rx_fifo_threshold(sl_ssi_handle_t ssi_handle)

To fetch the receiver FIFO threshold value, this value controls the level of entries at which the receive FIFO controller triggers an interrupt.

uint32_t
sl_si91x_ssi_get_receiver_sample_delay(sl_ssi_handle_t ssi_handle)

To fetch the receiver sample delay value, it used to delay the sample of the RX input signal.

__STATIC_INLINE sl_status_t

Set the secondary number in multi-secondary operation.

Enumeration Documentation#

ssi_event_typedef_t#

ssi_event_typedef_t

Enumeration for different SSI callback events.

Enumerator
SSI_EVENT_TRANSFER_COMPLETE

Transfer complete event.

SSI_EVENT_DATA_LOST

Data lost event.

SSI_EVENT_MODE_FAULT

Mode fault event.


ssi_peripheral_clock_mode_t#

ssi_peripheral_clock_mode_t

Enumeration for different SSI peripheral clock modes.

Enumerator
SL_SSI_PERIPHERAL_CPOL0_CPHA0

Mode 0 (CPOL = 0, CPHA = 0)

SL_SSI_PERIPHERAL_CPOL0_CPHA1

Mode 1 (CPOL = 0, CPHA = 1)

SL_SSI_PERIPHERAL_CPOL1_CPHA0

Mode 2 (CPOL = 1, CPHA = 0)

SL_SSI_PERIPHERAL_CPOL1_CPHA1

Mode 3 (CPOL = 1, CPHA = 1)

SL_SSI_PERIPHERAL_TI_SSI

TI mode.

SL_SSI_PERIPHERAL_MICROWIRE

Microwire/Half_duplex mode.

SL_SSI_PERIPHERAL_MODE_LAST

LSAT member of enum for validation.


sl_ssi_instance_t#

sl_ssi_instance_t

Enumeration for different SSI peripheral device modes.

Enumerator
SL_SSI_MASTER_ACTIVE

Primary mode is active.

SL_SSI_SLAVE_ACTIVE

Secondary mode is active.

SL_SSI_ULP_MASTER_ACTIVE

ULP PRIMARY mode is active.

SL_SSI_INSTANCE_LAST

LSAT member of enum for validation.


sl_ssi_slave_number_t#

sl_ssi_slave_number_t

Enumeration for SSI Secondary numbers.

Enumerator
SSI_SLAVE_0

Secondary No. 1.

SSI_SLAVE_1

Secondary No. 2.

SSI_SLAVE_2

Secondary No. 3.

SSI_SLAVE_3

Secondary No. 4.

SSI_SLAVE_NUMBER_LAST_ENUM

Last member of enum for validation.


Typedef Documentation#

sl_ssi_power_state_t#

typedef ARM_POWER_STATE sl_ssi_power_state_t

renaming arm power state structure


sl_ssi_status_t#

typedef ARM_SPI_STATUS sl_ssi_status_t

renaming arm SPI status


sl_ssi_driver_t#

typedef ARM_DRIVER_SPI sl_ssi_driver_t

Renaming SSI driver structure.


sl_ssi_handle_t#

typedef const void* sl_ssi_handle_t

SSI Handle to be passed into APIs.


sl_ssi_signal_event_t#

typedef ARM_SPI_SignalEvent_t sl_ssi_signal_event_t

Callback typedef for SSI.


Variable Documentation#

release#

uint8_t sl_ssi_version_t::release

Release version number.


major#

uint8_t sl_ssi_version_t::major

SQA version number.


minor#

uint8_t sl_ssi_version_t::minor

DEV version number.


bit_width#

uint8_t sl_ssi_control_config_t::bit_width

bit width either 8 or 16 bit


device_mode#

uint32_t sl_ssi_control_config_t::device_mode

mode such as Master or Slave mode


clock_mode#

uint32_t sl_ssi_control_config_t::clock_mode

clock mode such as CPOL0 CPHA1


baud_rate#

uint32_t sl_ssi_control_config_t::baud_rate

baud rate for SSI


receive_sample_delay#

uint32_t sl_ssi_control_config_t::receive_sample_delay

Delay for receive input signal.


division_factor#

uint16_t sl_ssi_clock_config_t::division_factor

Clock Division Factor.


intf_pll_500_control_value#

uint16_t sl_ssi_clock_config_t::intf_pll_500_control_value

intf PLL control value


intf_pll_clock#

uint32_t sl_ssi_clock_config_t::intf_pll_clock

intf PLL clock frequency


intf_pll_reference_clock#

uint32_t sl_ssi_clock_config_t::intf_pll_reference_clock

intf PLL reference clock frequency


soc_pll_clock#

uint32_t sl_ssi_clock_config_t::soc_pll_clock

SoC PLL Clock frequency.


soc_pll_reference_clock#

uint32_t sl_ssi_clock_config_t::soc_pll_reference_clock

SoC PLL reference clock frequency.


soc_pll_mm_count_value#

uint8_t sl_ssi_clock_config_t::soc_pll_mm_count_value

SoC PLL count value.


Function Documentation#

sl_si91x_ssi_configure_clock#

sl_status_t sl_si91x_ssi_configure_clock (sl_ssi_clock_config_t * clock_config)

Set the clock for the SSI peripheral, Configures the PLL clock and SOC clock with the value set by user in the clock configuration structure.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_clock_config_t *[in]clock_config

Pointer to clock config structure sl_ssi_clock_config_t

Returns

  • status 0 if successful, else error code as follow.

    • SL_STATUS_OK (0x0000) - Success, timer clock-source parameters configured properly

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_FAIL (0x0001) - The function is failed

    • SL_STATUS_NOT_INITIALIZED (0x0011) - Clock is not initialized


sl_si91x_ssi_init#

sl_status_t sl_si91x_ssi_init (sl_ssi_instance_t instance, sl_ssi_handle_t * ssi_handle)

Initialize the SSI.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_instance_t[in]instance

(Primary/Secondary/ULP Primary) ( sl_ssi_instance_t)

sl_ssi_handle_t *[in]ssi_handle

Double Pointer to the SSI driver handle ( sl_ssi_handle_t)

If the DMA is enabled, it also initializes the DMA. Pass the address of the pointer for storing the SSI Primary/Secondary/ULP Primary handle, which can be used in future for other function calls.

Returns

  • status 0 if successful, else error code as follow.

    • SL_STATUS_OK (0x0000) - Success, otherwise fail error code as follow

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_ssi_deinit#

sl_status_t sl_si91x_ssi_deinit (sl_ssi_handle_t ssi_handle)

Uninitialize the SSI.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

If the DMA is enabled, it also uninitializes the DMA

Returns

  • status 0 if successful, else error code as follow.

    • SL_STATUS_OK (0x0000) - Success, otherwise fail error code as follow

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer


sl_si91x_ssi_set_configuration#

sl_status_t sl_si91x_ssi_set_configuration (sl_ssi_handle_t ssi_handle, sl_ssi_control_config_t * control_configuration, sl_ssi_slave_number_t slave_number)

Control and configure the SSI.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

pointer to ssi instance handle. ( sl_ssi_handle_t)

sl_ssi_control_config_t *[in]control_configuration

pointer to control config structure. ( sl_ssi_control_config_t)

sl_ssi_slave_number_t[in]slave_number

In the current implementation variable slave_number is un-used ( sl_ssi_slave_number_t)

  • Mode (Primary/Secondary/ULP Primary)

  • bit_width (4 bit to 16 bit)

  • clock_mode/Frame format (mode0 to mode3, TI and Microwire)

  • bitrate (10 Mbps to 40 Mbps)

  • Rx sample delay (0 to 63)

Returns

  • status 0 if successful, else error code as follow.

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_FAIL (0x0001) - The function is failed

    • SL_STATUS_NOT_SUPPORTED (0x000F) - Parameter is not supported

    • SL_STATUS_BUSY (0x0004) - Driver is busy

    • SL_STATUS_INVALID_MODE (0x0024) - Slave select Mode is invalid

    • SL_STATUS_INVALID_TYPE (0x0026) - SPI frame format is not valid

    • SL_STATUS_INVALID_RANGE (0x0028) - Data bits (frame length) is not in range


sl_si91x_ssi_receive_data#

sl_status_t sl_si91x_ssi_receive_data (sl_ssi_handle_t ssi_handle, void * data, uint32_t data_length)

Start receiving the data from the SSI interface.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

void *[in]data

pointer to the variable which will store the received data

uint32_t[in]data_length

(uint32_t) number of data items to receive

Returns

  • status 0 if successful, else error code as follow.

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_FAIL (0x0001) - The function is failed

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_ssi_send_data#

sl_status_t sl_si91x_ssi_send_data (sl_ssi_handle_t ssi_handle, const void * data, uint32_t data_length)

Start sending the data from the SSI interface.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

const void *[in]data

pointer to the variable which will store the received data

uint32_t[in]data_length

(uint32_t) number of data items to receive

Returns

  • status 0 if successful, else error code as follow.

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_FAIL (0x0001) - The function is failed

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_ssi_transfer_data#

sl_status_t sl_si91x_ssi_transfer_data (sl_ssi_handle_t ssi_handle, const void * data_out, void * data_in, uint32_t data_length)

Start to send and receive bi-directional full duplex data to/from the SPI secondary.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

const void *[in]data_out

const pointer to the variable that has data which needs to be sent

void *[in]data_in

pointer to the variable which will store the received data

uint32_t[in]data_length

(uint32_t) number of data items to receive

Returns

  • status 0 if successful, else error code

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid

    • SL_STATUS_FAIL (0x0001) - The function is failed

    • SL_STATUS_BUSY (0x0004) - Driver is busy


sl_si91x_ssi_get_status#

sl_ssi_status_t sl_si91x_ssi_get_status (sl_ssi_handle_t ssi_handle)

Get the SSI status.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

Get the transfer status SSI.

Returns

  • busy, data lost or mode fault returns as a bit field.

It returns the sl_ssi_status_t type structure. The members are:

  • Busy

  • Data Lost

  • Mode Fault It is generally used to poll the busy status of SSI Master/ULP Master.

Returns


sl_si91x_ssi_get_version#

sl_ssi_version_t sl_si91x_ssi_get_version (void )

Get the SSI version.

Parameters
TypeDirectionArgument NameDescription
void[in]

It returns the API version of SSI.

Returns

  • driver version.


sl_si91x_ssi_get_rx_data_count#

uint32_t sl_si91x_ssi_get_rx_data_count (sl_ssi_handle_t ssi_handle)

Get data receive count of the SSI.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

It returns the number of data received at the time of function call.

Returns

  • uint32_t value of the RX data count


sl_si91x_ssi_get_tx_data_count#

uint32_t sl_si91x_ssi_get_tx_data_count (sl_ssi_handle_t ssi_handle)

Get the transmit data count of SSI.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

It returns the number of data transmit at the time of function call

Returns

  • uint32_t value of the tx data count


sl_si91x_ssi_register_event_callback#

sl_status_t sl_si91x_ssi_register_event_callback (sl_ssi_handle_t ssi_handle, sl_ssi_signal_event_t callback_event)

Register the user event callback.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

handle Pointer to the SSI driver handle ( sl_ssi_handle_t)

sl_ssi_signal_event_t[in]callback_event

Pointer to the function which needs to be called at the time of interrupt

It registers the callback, i.e., stores the callback function address and pass to the variable that is called in Interrupt Handler. If another callback is registered without unregistering previous callback then, it returns an error code as follow, so it is mandatory to unregister the callback before registering another callback.

Returns

  • status 0 if successful, else error code as follow.

    • SL_STATUS_BUSY (0x0004) - The callback is already registered, unregister previous callback before registering new one.

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer


sl_si91x_ssi_unregister_event_callback#

void sl_si91x_ssi_unregister_event_callback (void )

Unregister the user event callback.

Parameters
TypeDirectionArgument NameDescription
void[in]

It unregisters the callback, i.e., clears the callback function address and passes a NULL value to the variable.


sl_si91x_ssi_get_clock_division_factor#

uint32_t sl_si91x_ssi_get_clock_division_factor (sl_ssi_handle_t ssi_handle)

Fetch the clock division factor.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

Returns

  • factor(int32_t) The value of clock division fac


sl_si91x_ssi_get_frame_length#

uint32_t sl_si91x_ssi_get_frame_length (sl_ssi_handle_t ssi_handle)

Fetch the frame length i.e., bit width.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

The frame length ranges between 4 and 16.

Returns

  • frame_length (uint32_t) The value of frame length


sl_si91x_ssi_get_tx_fifo_threshold#

uint32_t sl_si91x_ssi_get_tx_fifo_threshold (sl_ssi_handle_t ssi_handle)

To fetch the transmit FIFO threshold value, this value controls the level of entries at which the transmit FIFO controller triggers an interrupt.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

Returns

  • Transmit fifo threshold (uint32_t) The value of transmit fifo threshold


sl_si91x_ssi_get_rx_fifo_threshold#

uint32_t sl_si91x_ssi_get_rx_fifo_threshold (sl_ssi_handle_t ssi_handle)

To fetch the receiver FIFO threshold value, this value controls the level of entries at which the receive FIFO controller triggers an interrupt.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

Returns

  • Receiver fifo threshold (uint32_t) The value of receiver fifo threshold


sl_si91x_ssi_get_receiver_sample_delay#

uint32_t sl_si91x_ssi_get_receiver_sample_delay (sl_ssi_handle_t ssi_handle)

To fetch the receiver sample delay value, it used to delay the sample of the RX input signal.

Parameters
TypeDirectionArgument NameDescription
sl_ssi_handle_t[in]ssi_handle

Pointer to the SSI driver handle ( sl_ssi_handle_t)

Each value represents a single ssi_clk delay on the sample of the rxd signal.

Returns

  • Receiver sample delay (uint32_t) The value of receiver sample delay


sl_si91x_ssi_set_slave_number#

__STATIC_INLINE sl_status_t sl_si91x_ssi_set_slave_number (uint8_t number)

Set the secondary number in multi-secondary operation.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]number

Secondary number ( sl_ssi_slave_number_t )

For single secondary also, this API needs to be called before transferring the data.

Returns

  • none