Watchdog Timer#
Modules#
Enumerations#
Enumeration to represent possible time delays values for WDT interrupt time and system reset time with 32 KHZ clock freq.
Typedefs#
Typedef for the function pointer of the callback function.
Renaming high frequency fsm-clock type enum.
Renaming low frequency fsm-clock type enum.
Functions#
Initialize the Watchdog timer by enabling the peripheral power.
Enables and configures the timer clock sources.
Configures the watchdog timer parameters.
Registers the Watchdog timer timeout callback.
Sets the Watchdog timer interrupt time (overflow or restart time).
Reads the Watchdog timer interrupt time set value.
Sets the Watchdog timer system-reset time duration.
Reads the Watchdog timer system-reset time set value It will return system reset time in terms of power of two.
Sets the Watchdog timer window time value By setting this value timer becomes as Window watchdog timer, if this value is zero it act as usual WDT.
Reads the Watchdog timer window time set value.
Reads the Watchdog timer system-reset status.
De-initializes the Watchdog timer, mask its interrupt, de-power and disable timer.
Unregisters the Watchdog timer timeout callback.
Gets the Watchdog timer version.
Starts and enables the Watchdog timer.
Stops the Watchdog timer by disabling it.
Restarts (kick) an already running Watchdog timer.
Enables the Watchdog timer to reset the system on processor lockup.
Disables the watchdog timer to reset system on processor lockup or on processor stuck.
Enumeration Documentation#
bg_pmu_clock_t#
bg_pmu_clock_t
Enumeration to represent bg-pmu clock sources.
| Enumerator | |
|---|---|
| RO_32KHZ_CLOCK | RO_32KHz_clock. |
| MCU_FSM__CLOCK | mcu_fsm__clock |
time_delays_t#
time_delays_t
Enumeration to represent possible time delays values for WDT interrupt time and system reset time with 32 KHZ clock freq.
| Enumerator | |
|---|---|
| TIME_DELAY_0 | for time delay of 0.03125 milliseconds |
| TIME_DELAY_1 | for time delay of 0.0625 milliseconds |
| TIME_DELAY_2 | for time delay of 0.125 milliseconds |
| TIME_DELAY_3 | for time delay of 0.25 milliseconds |
| TIME_DELAY_4 | for time delay of 0.5 milliseconds |
| TIME_DELAY_5 | for time delay of 1 milliseconds |
| TIME_DELAY_6 | for time delay of 2 milliseconds |
| TIME_DELAY_7 | for time delay of 4 milliseconds |
| TIME_DELAY_8 | for time delay of 8 milliseconds |
| TIME_DELAY_9 | for time delay of 16 milliseconds |
| TIME_DELAY_10 | for time delay of 32 milliseconds |
| TIME_DELAY_11 | for time delay of 64 milliseconds |
| TIME_DELAY_12 | for time delay of 128 milliseconds |
| TIME_DELAY_13 | for time delay of 256 milliseconds |
| TIME_DELAY_14 | for time delay of 512 milliseconds |
| TIME_DELAY_15 | for time delay of 1.024 seconds |
| TIME_DELAY_16 | for time delay of 2.048 seconds |
| TIME_DELAY_17 | for time delay of 4.096 seconds |
| TIME_DELAY_18 | for time delay of 8.192 seconds |
| TIME_DELAY_19 | for time delay of 16.384 seconds |
| TIME_DELAY_20 | for time delay of 32.768 seconds |
| TIME_DELAY_21 | for time delay of 65.536 seconds |
| TIME_DELAY_22 | for time delay of 131.072 seconds |
| TIME_DELAY_23 | for time delay of 262.144 seconds |
| TIME_DELAY_24 | for time delay of 524.288 seconds |
| TIME_DELAY_25 | for time delay of 1048.576 seconds |
| TIME_DELAY_26 | for time delay of 2097.152 seconds |
| TIME_DELAY_27 | for time delay of 4194.304 seconds |
| TIME_DELAY_28 | for time delay of 8388.60 seconds |
| TIME_DELAY_29 | for time delay of 16777.216 seconds |
| TIME_DELAY_30 | for time delay of 33554.432 seconds |
| TIME_DELAY_31 | for time delay of 67108.864 seconds |
| TIME_DELAY_LAST | for time delay value validation |
Typedef Documentation#
watchdog_timer_callback_t#
typedef void(* watchdog_timer_callback_t) (void) )(void)
Typedef for the function pointer of the callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | data | (void *)extra parameter for user application |
high_freq_fsm_clock_t#
typedef FSM_CLK_T high_freq_fsm_clock_t
Renaming high frequency fsm-clock type enum.
low_freq_fsm_clock_t#
typedef AON_CLK_T low_freq_fsm_clock_t
Renaming low frequency fsm-clock type enum.
Function Documentation#
sl_si91x_watchdog_init_timer#
void sl_si91x_watchdog_init_timer (void )
Initialize the Watchdog timer by enabling the peripheral power.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Also enables it to run during sleep mode). Also un-masks its interrupt.
Returns
none
sl_si91x_watchdog_configure_clock#
sl_status_t sl_si91x_watchdog_configure_clock (watchdog_timer_clock_config_t * timer_clk_config_ptr)
Enables and configures the timer clock sources.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| watchdog_timer_clock_config_t * | [in] | timer_clk_config_ptr | Pointer to timer clock configuration structure |
Configures the watchdog-timer low frequency, high frequency and bg-pmu clock sources.
Pre-conditions:
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - Timer configuration structure members have invalid values, for members watchdog_timer_clock_config_t
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success, timer clock-source parameters configured properly
sl_si91x_watchdog_set_configuration#
sl_status_t sl_si91x_watchdog_set_configuration (watchdog_timer_config_t * timer_config_ptr)
Configures the watchdog timer parameters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| watchdog_timer_config_t * | [in] | timer_config_ptr | Pointer to timer clock configuration structure |
Parameters are interrupt time (WDT restart time), system reset time & window time (lower time stamp for WDT restart, if required). System reset time should be greater than interrupt time. And Interrupt time should be greater than window time, else API will give error.
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - Timer configuration structure members have invalid values, for members watchdog_timer_config_t
SL_STATUS_INVALID_CONFIGURATION (0x0023) - Timer configuration structure member 'system_reset_time' is less than or equal to 'interrupt_time'. It should be greater than interrupt time of timer.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success, timer parameters configured properly
sl_si91x_watchdog_register_timeout_callback#
sl_status_t sl_si91x_watchdog_register_timeout_callback (watchdog_timer_callback_t on_timeout_callback)
Registers the Watchdog timer timeout callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| watchdog_timer_callback_t | [in] | on_timeout_callback | (function pointer) Callback function pointer to be called when timer timeout interrupt occurred. |
Also enables its interrupts. If any callback is already registered, the user needs to unregister the callback first before registering the callback.
Returns
status 0 if successful, else error code as follows:
SL_STATUS_NULL_POINTER (0x0022) - Callback function pointer parameter is a null pointer.
SL_STATUS_BUSY (0x0004) - The callback is already registered, the user must unregister the previous callback before registering again
SL_STATUS_OK (0x0000) - Successfully registered timer timer-out callback
sl_si91x_watchdog_set_interrupt_time#
sl_status_t sl_si91x_watchdog_set_interrupt_time (time_delays_t interrupt_time)
Sets the Watchdog timer interrupt time (overflow or restart time).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_delays_t | [in] | interrupt_time | (time_delays_t), timer timeout interrupt duration, Number of clock pulses = 2^(interrupt_time), time_delays_t |
This also referred as upper time-stamp for WDT restart Its maximum value is 31. Number of clock pulses for timer timeout = 2^(interrupt_time) This value should be less than system-reset time and greater than window time.
Pre-conditions:
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - 'interrupt_time' parameter has an invalid value.
SL_STATUS_INVALID_CONFIGURATION (0x0023) - 'interrupt_time' value is less than window time or greater than system reset time
SL_STATUS_OK (0x0000) - Successfully set watchdog timer timeout time value
sl_si91x_watchdog_get_interrupt_time#
uint8_t sl_si91x_watchdog_get_interrupt_time (void )
Reads the Watchdog timer interrupt time set value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
It will return interrupt time in terms of power of two.
Pre-conditions:
Returns
returns interrupt time (uint8_t) value, time_delays_t
sl_si91x_watchdog_set_system_reset_time#
sl_status_t sl_si91x_watchdog_set_system_reset_time (time_delays_t system_reset_time)
Sets the Watchdog timer system-reset time duration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_delays_t | [in] | system_reset_time | (time_delays_t) timer system-reset duration, Number of clock pulses = 2^(system_reset_time), time_delays_t |
Its maximum value is 31. Number of clock pulses for system reset time = 2^(system_reset_time). This value should be greater than timer interrupt time & window time.
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - 'system_reset_time' parameter has an invalid value.
SL_STATUS_INVALID_CONFIGURATION (0x0023) - 'system_reset_time' value is less than window time or interrupt time
SL_STATUS_OK (0x0000) - Successfully set watchdog timer system-reset time value
sl_si91x_watchdog_get_system_reset_time#
uint8_t sl_si91x_watchdog_get_system_reset_time (void )
Reads the Watchdog timer system-reset time set value It will return system reset time in terms of power of two.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
returns system-reset time (uint8_t) value, time_delays_t
sl_si91x_watchdog_set_window_time#
sl_status_t sl_si91x_watchdog_set_window_time (time_delays_t window_time)
Sets the Watchdog timer window time value By setting this value timer becomes as Window watchdog timer, if this value is zero it act as usual WDT.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_delays_t | [in] | window_time | (time_delays_t), timer window time, Number of clock pulses = 2^(window_time),time_delays_t |
It is also referred as lower time-stamp for WDT restart. Its maximum value is 15. Number of clock pulses for window time = 2^(window_time). This value should be less than timer interrupt time and system-reset time.
Pre-conditions:
Returns
status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - 'window_time' parameter has an invalid value.
SL_STATUS_INVALID_CONFIGURATION (0x0023) - 'window_time' value is greater than interrupt time or system reset time
SL_STATUS_OK (0x0000) - Successfully set watchdog timer window time value
sl_si91x_watchdog_get_window_time#
uint8_t sl_si91x_watchdog_get_window_time (void )
Reads the Watchdog timer window time set value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
It returns time in terms of power of two.
Pre-conditions:
Returns
returns window time (uint8_t) value, time_delays_t
sl_si91x_watchdog_get_timer_system_reset_status#
boolean_t sl_si91x_watchdog_get_timer_system_reset_status (void )
Reads the Watchdog timer system-reset status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
This will return true when watchdog-timer resets system and returns false when it is a power-on reset.
Returns
returns true if watchdog timer resets system, else returns false
sl_si91x_watchdog_deinit_timer#
void sl_si91x_watchdog_deinit_timer (void )
De-initializes the Watchdog timer, mask its interrupt, de-power and disable timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Returns
none
Note
Unregisters the timer callback.
sl_si91x_watchdog_unregister_timeout_callback#
void sl_si91x_watchdog_unregister_timeout_callback (void )
Unregisters the Watchdog timer timeout callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
It will unregister the callback, i.e., clear the callback function address and pass NULL value to the variable.
Pre-conditions:
Returns
none
sl_si91x_watchdog_get_version#
sl_watchdog_timer_version_t sl_si91x_watchdog_get_version ( none)
Gets the Watchdog timer version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | none |
It returns the API version of watchdog timer.
Returns
(sl_watchdog_version_t) type structure
sl_si91x_watchdog_start_timer#
__STATIC_INLINE void sl_si91x_watchdog_start_timer (void )
Starts and enables the Watchdog timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Once WDT is started interrupt time will start incrementing as it reaches set interrupt time value, WDT will generate interrupt and timer will load system reset time value and before it reaches this value WDT should be restarted (kicked) to avoid System reset.
Pre-conditions:
Returns
none
sl_si91x_watchdog_stop_timer#
__STATIC_INLINE void sl_si91x_watchdog_stop_timer (void )
Stops the Watchdog timer by disabling it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Used to stop an already running timer.
Pre-conditions:
Returns
none
sl_si91x_watchdog_restart_timer#
__STATIC_INLINE void sl_si91x_watchdog_restart_timer (void )
Restarts (kick) an already running Watchdog timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
It should be used for already running WDT timer, not for starting a stopped timer.
Pre-conditions:
Returns
none
sl_si91x_watchdog_enable_system_reset_on_processor_lockup#
__STATIC_INLINE void sl_si91x_watchdog_enable_system_reset_on_processor_lockup (void )
Enables the Watchdog timer to reset the system on processor lockup.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none
sl_si91x_watchdog_disable_system_reset_on_processor_lockup#
__STATIC_INLINE void sl_si91x_watchdog_disable_system_reset_on_processor_lockup (void )
Disables the watchdog timer to reset system on processor lockup or on processor stuck.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
Pre-conditions:
Returns
none