Wi-Fi Access Point configuration.
Public Attributes#
SSID.
Security mode.
Encryption mode.
Channel.
Rate protocol.
Optional flags for AP configuration.
ID of secure credentials.
Keep alive type of the access point. One of the values from sl_si91x_ap_keepalive_type_t
Beacon interval of the access point in milliseconds.
Duration in milliseconds to kick idle client.
How many beacons per DTIM.
Maximum number of associated clients.
Stop beaconing when there are no associated clients.
To enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.
A flag to enable 11n.
Public Attribute Documentation#
ssid#
sl_wifi_ssid_t sl_wifi_ap_configuration_t::ssid
SSID.
176
of file components/protocol/wifi/inc/sl_wifi_types.h
security#
sl_wifi_security_t sl_wifi_ap_configuration_t::security
Security mode.
177
of file components/protocol/wifi/inc/sl_wifi_types.h
encryption#
sl_wifi_encryption_t sl_wifi_ap_configuration_t::encryption
Encryption mode.
178
of file components/protocol/wifi/inc/sl_wifi_types.h
channel#
sl_wifi_channel_t sl_wifi_ap_configuration_t::channel
Channel.
179
of file components/protocol/wifi/inc/sl_wifi_types.h
rate_protocol#
sl_wifi_rate_protocol_t sl_wifi_ap_configuration_t::rate_protocol
Rate protocol.
180
of file components/protocol/wifi/inc/sl_wifi_types.h
options#
sl_wifi_ap_flag_t sl_wifi_ap_configuration_t::options
Optional flags for AP configuration.
181
of file components/protocol/wifi/inc/sl_wifi_types.h
credential_id#
sl_wifi_credential_id_t sl_wifi_ap_configuration_t::credential_id
ID of secure credentials.
182
of file components/protocol/wifi/inc/sl_wifi_types.h
keepalive_type#
uint8_t sl_wifi_ap_configuration_t::keepalive_type
Keep alive type of the access point. One of the values from sl_si91x_ap_keepalive_type_t
184
of file components/protocol/wifi/inc/sl_wifi_types.h
beacon_interval#
uint16_t sl_wifi_ap_configuration_t::beacon_interval
Beacon interval of the access point in milliseconds.
185
of file components/protocol/wifi/inc/sl_wifi_types.h
client_idle_timeout#
uint32_t sl_wifi_ap_configuration_t::client_idle_timeout
Duration in milliseconds to kick idle client.
186
of file components/protocol/wifi/inc/sl_wifi_types.h
dtim_beacon_count#
uint16_t sl_wifi_ap_configuration_t::dtim_beacon_count
How many beacons per DTIM.
187
of file components/protocol/wifi/inc/sl_wifi_types.h
maximum_clients#
uint8_t sl_wifi_ap_configuration_t::maximum_clients
Maximum number of associated clients.
188
of file components/protocol/wifi/inc/sl_wifi_types.h
beacon_stop#
uint8_t sl_wifi_ap_configuration_t::beacon_stop
Stop beaconing when there are no associated clients.
189
of file components/protocol/wifi/inc/sl_wifi_types.h
tdi_flags#
sl_wifi_tdi_t sl_wifi_ap_configuration_t::tdi_flags
To enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.
190
of file components/protocol/wifi/inc/sl_wifi_types.h
is_11n_enabled#
uint8_t sl_wifi_ap_configuration_t::is_11n_enabled
A flag to enable 11n.
191
of file components/protocol/wifi/inc/sl_wifi_types.h