Wi-Fi device status.

Public Attributes#

uint8_t

WiFi Client active.

uint8_t

WiFi Access point active.

uint8_t

WiFi promiscuous mode active.

uint8_t

Reserved Status bit.

uint8_t

Reserved Status bit.

uint8_t

Scan in Progress.

uint8_t

Reserved Status bit.

uint8_t

Reserved Status bit.

Public Attribute Documentation#

client_active#

uint8_t sl_wifi_status_t::client_active

WiFi Client active.


Definition at line 351 of file components/protocol/wifi/inc/sl_wifi_types.h

ap_active#

uint8_t sl_wifi_status_t::ap_active

WiFi Access point active.


Definition at line 352 of file components/protocol/wifi/inc/sl_wifi_types.h

monitor_mode_active#

uint8_t sl_wifi_status_t::monitor_mode_active

WiFi promiscuous mode active.


Definition at line 353 of file components/protocol/wifi/inc/sl_wifi_types.h

wfd_go_active#

uint8_t sl_wifi_status_t::wfd_go_active

Reserved Status bit.


Definition at line 354 of file components/protocol/wifi/inc/sl_wifi_types.h

wfd_client_active#

uint8_t sl_wifi_status_t::wfd_client_active

Reserved Status bit.


Definition at line 355 of file components/protocol/wifi/inc/sl_wifi_types.h

scan_active#

uint8_t sl_wifi_status_t::scan_active

Scan in Progress.


Definition at line 356 of file components/protocol/wifi/inc/sl_wifi_types.h

_reserved#

uint8_t sl_wifi_status_t::_reserved

Reserved Status bit.


Definition at line 357 of file components/protocol/wifi/inc/sl_wifi_types.h

_reserved2#

uint8_t sl_wifi_status_t::_reserved2

Reserved Status bit.


Definition at line 358 of file components/protocol/wifi/inc/sl_wifi_types.h