Wi-Fi max transmit power.

Public Attributes#

uint8_t

Transmit power during scan. Valid input range: 1dBm to 31dBm.

uint8_t

Transmit power during join. Valid input range: 1dBm to 31dBm.

Public Attribute Documentation#

scan_tx_power#

uint8_t sl_wifi_max_tx_power_t::scan_tx_power

Transmit power during scan. Valid input range: 1dBm to 31dBm.


join_tx_power#

uint8_t sl_wifi_max_tx_power_t::join_tx_power

Transmit power during join. Valid input range: 1dBm to 31dBm.