Structure to hold the fifo threshold configuration parameters.

Public Attributes#

uint8_t

Number of channel enable.

uint8_t

AEMPTY Threshold.

uint8_t

AFULL Threshold.

uint8_t

Internal or External DMA.

Public Attribute Documentation#

num_of_channel_en#

uint8_t sl_adc_fifo_thrld_config_t::num_of_channel_en

Number of channel enable.


a_empty_threshold#

uint8_t sl_adc_fifo_thrld_config_t::a_empty_threshold

AEMPTY Threshold.


a_full_threshold#

uint8_t sl_adc_fifo_thrld_config_t::a_full_threshold

AFULL Threshold.


dma_type#

uint8_t sl_adc_fifo_thrld_config_t::dma_type

Internal or External DMA.