Wi-Fi Client interface advance configuration.

Public Attributes#

uint32_t

Maximum number of retries before indicating join failure.

uint32_t

Scan interval in seconds between each retry.

uint32_t

Number of missed beacons that will trigger rejoin.

uint32_t

Retry enable or disable for first time joining.

Public Attribute Documentation#

max_retry_attempts#

uint32_t sl_wifi_advanced_client_configuration_t::max_retry_attempts

Maximum number of retries before indicating join failure.


scan_interval#

uint32_t sl_wifi_advanced_client_configuration_t::scan_interval

Scan interval in seconds between each retry.


beacon_missed_count#

uint32_t sl_wifi_advanced_client_configuration_t::beacon_missed_count

Number of missed beacons that will trigger rejoin.


first_time_retry_enable#

uint32_t sl_wifi_advanced_client_configuration_t::first_time_retry_enable

Retry enable or disable for first time joining.