Wi-Fi buffer configuration.
Public Attributes#
uint8_t
Indicates the limit on buffers used for sending data to TA.
uint8_t
Indicates the limit on buffers used for storing response from TA.
uint8_t
Indicates the limit on buffers used for sending command to TA.
uint32_t
Indicates the block size.
void *
This field points to the chunk of memory allocated on first invocation of malloc.
Public Attribute Documentation#
tx_buffer_quota#
uint8_t sl_wifi_buffer_configuration_t::tx_buffer_quota
Indicates the limit on buffers used for sending data to TA.
rx_buffer_quota#
uint8_t sl_wifi_buffer_configuration_t::rx_buffer_quota
Indicates the limit on buffers used for storing response from TA.
control_buffer_quota#
uint8_t sl_wifi_buffer_configuration_t::control_buffer_quota
Indicates the limit on buffers used for sending command to TA.
buffer_memory#
void* sl_wifi_buffer_configuration_t::buffer_memory
This field points to the chunk of memory allocated on first invocation of malloc.