Public Attributes#

uint8_t

Min contention window size. Value is calculated from 2n - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.

uint8_t

Max contention window size. Value is calculated from 2n - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.

uint8_t

AIFSN. Valid range is 0 to 15.

uint8_t

Public Attribute Documentation#

cwmin#

uint8_t sl_wifi_transceiver_cw_config_t::cwmin

Min contention window size. Value is calculated from 2n - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.


cwmax#

uint8_t sl_wifi_transceiver_cw_config_t::cwmax

Max contention window size. Value is calculated from 2n - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.


aifsn#

uint8_t sl_wifi_transceiver_cw_config_t::aifsn

AIFSN. Valid range is 0 to 15.


reserved#

uint8_t sl_wifi_transceiver_cw_config_t::reserved