Wi-Fi Enterprise security credentials.

Public Attributes#

uint8_t

Enterprise User Name.

uint8_t

Enterprise password.

uint8_t

Certificate password.

uint32_t

Certificate Id for Enterprise authentication.

uint32_t

Public Attribute Documentation#

username#

uint8_t sl_wifi_eap_credential_t::username[SL_WIFI_EAP_USER_NAME_LENGTH]

Enterprise User Name.


password#

uint8_t sl_wifi_eap_credential_t::password[SL_WIFI_EAP_PASSWORD_LENGTH]

Enterprise password.


certificate_key#

uint8_t sl_wifi_eap_credential_t::certificate_key[SL_WIFI_EAP_CERTIFICATE_KEY_LENGTH]

Certificate password.


certificate_id#

uint32_t sl_wifi_eap_credential_t::certificate_id

Certificate Id for Enterprise authentication.


eap_flags#

uint32_t sl_wifi_eap_credential_t::eap_flags

EAP Flags of type sl_wifi_eap_client_flag_t.

Note

    • BIT[0] of Opportunistic Key Caching (OKC) is used to enable or disable OKC: –0 – disable; –1 – enable. When this is enabled, module will use cached PMKID to get the Master Session Key (MSK), which is needed for generating PMK that is needed for 4-way handshake.

    • BIT[1] of OKC is used to enable or disable CA certification for PEAP connection: –0 – CA certificate is not required; –1 – CA certificate is required.

    • BIT[2-12] of OKC argument are used for cipher list selection for EAP connection. All possible ciphers are listed below.

      BIT position

      Cipher selected

      2

      DHE-RSA-AES256-SHA256

      3

      DHE-RSA-AES128-SHA256

      4

      DHE-RSA-AES256-SHA

      5

      DHE-RSA-AES128-SHA

      6

      AES256-SHA256

      7

      AES128-SHA256

      8

      AES256-SHA

      9

      AES128-SHA

      10

      RC4-SHA

      11

      DES-CBC3-SHA

      12

      RC4-MD5

    • BIT[13-31] of OKC argument is reserved.

  • If a user sets BIT[1] and does not provide the CA certificate for PEAP connection, an error is thrown. If a user provides an invalid CA certificate, an error is also thrown. A user can set either one or multiple bits from BIT[2-12] to provide the cipher list. If a user does not provide any values in OKC BIT[2-12], all ciphers are selected by default.