Public Attributes#
uint8_t
Bit 0 is set to 1 to enable filtering for the specified MAC addresses, else set to 0 to disable filtering.
uint8_t
Number of multicast addresses. Valid values are 1, 2. This field is ignored when disabling filtering.
uint8_t
List of multicast addresses. This field is ignored when disabling filtering.
Public Attribute Documentation#
flags#
uint8_t sl_wifi_transceiver_mcast_filter_t::flags
Bit 0 is set to 1 to enable filtering for the specified MAC addresses, else set to 0 to disable filtering.
num_of_mcast_addr#
uint8_t sl_wifi_transceiver_mcast_filter_t::num_of_mcast_addr
Number of multicast addresses. Valid values are 1, 2. This field is ignored when disabling filtering.
mac#
uint8_t sl_wifi_transceiver_mcast_filter_t::mac[2][6]
List of multicast addresses. This field is ignored when disabling filtering.