Wi-Fi Client interface advanced configuration structure.
Public Attributes#
uint32_t
Maximum number of retries before indicating join failure.
uint32_t
Scan interval in seconds between each retry.
uint32_t
Number of missed beacons that will trigger rejoin.
uint32_t
Retry enable or disable for first time joining.
Public Attribute Documentation#
max_retry_attempts#
uint32_t sl_wifi_advanced_client_configuration_t::max_retry_attempts
Maximum number of retries before indicating join failure.
scan_interval#
uint32_t sl_wifi_advanced_client_configuration_t::scan_interval
Scan interval in seconds between each retry.
beacon_missed_count#
uint32_t sl_wifi_advanced_client_configuration_t::beacon_missed_count
Number of missed beacons that will trigger rejoin.
first_time_retry_enable#
uint32_t sl_wifi_advanced_client_configuration_t::first_time_retry_enable
Retry enable or disable for first time joining.