Wi-Fi transceiver peer update structure.

Defines the configuration parameters for adding or deleting a peer in the Wi-Fi transceiver. The peer can be added or deleted based on the MAC address.

Public Attributes#

uint8_t
uint8_t

MAC address of peer to be added or deleted.

uint32_t

Rate bitmap of peer station.

Public Attribute Documentation#

flags#

uint8_t sl_wifi_transceiver_peer_update_t::flags

Bit position

Flags bit description

0

Shall be set to add the peer, else reset to 0 to delete the peer.

1

Shall be set for auto-rate enable. To enable auto-rate, application needs to provide peer_supported_rate_bitmap


peer_mac_address#

uint8_t sl_wifi_transceiver_peer_update_t::peer_mac_address[6]

MAC address of peer to be added or deleted.


peer_supported_rate_bitmap#

uint32_t sl_wifi_transceiver_peer_update_t::peer_supported_rate_bitmap

Rate bitmap of peer station.

peer_supported_rate_bitmap

Data rate

BIT(0)

1 Mbps

BIT(1)

2 Mbps

BIT(2)

5.5 Mbps

BIT(3)

11 Mbps

BIT(4)

6 Mbps

BIT(5)

9 Mbps

BIT(6)

12 Mbps

BIT(7)

18 Mbps

BIT(8)

24 Mbps

BIT(9)

36 Mbps

BIT(10)

48 Mbps

BIT(11)

54 Mbps

BIT(12:31)

Reserved