Wi-Fi device status structure.

Indicates the status of various Wi-Fi functionalities on the device. It uses bit fields to indicate the status of different Wi-Fi modes and operations.

Public Attributes#

uint8_t

WiFi Client active.

uint8_t

WiFi Access point active.

uint8_t

WiFi promiscuous mode active.

uint8_t

Reserved Status bit.

uint8_t

Reserved Status bit.

uint8_t

Scan in Progress.

uint8_t

Reserved Status bit.

uint8_t

Reserved Status bit.

Public Attribute Documentation#

client_active#

uint8_t sl_wifi_status_t::client_active

WiFi Client active.


ap_active#

uint8_t sl_wifi_status_t::ap_active

WiFi Access point active.


monitor_mode_active#

uint8_t sl_wifi_status_t::monitor_mode_active

WiFi promiscuous mode active.


wfd_go_active#

uint8_t sl_wifi_status_t::wfd_go_active

Reserved Status bit.


wfd_client_active#

uint8_t sl_wifi_status_t::wfd_client_active

Reserved Status bit.


scan_active#

uint8_t sl_wifi_status_t::scan_active

Scan in Progress.


_reserved#

uint8_t sl_wifi_status_t::_reserved

Reserved Status bit.


_reserved2#

uint8_t sl_wifi_status_t::_reserved2

Reserved Status bit.