You are viewing documentation for version:
Structure representing a Wi-Fi buffer.
Public Attributes#
sl_slist_node_t
Pointer to the node of the list of which the buffer is part of.
uint32_t
Size of the buffer in bytes.
uint8_t
Indicates the buffer type (SL_WIFI_TX_FRAME_BUFFER, SL_WIFI_RX_FRAME_BUFFER, and so on.) corresponding to the buffer.
uint8_t
Stores the data (header + payload) to be send to NWP.
Public Attribute Documentation#
node#
sl_slist_node_t sl_wifi_buffer_t::node
Pointer to the node of the list of which the buffer is part of.
length#
uint32_t sl_wifi_buffer_t::length
Size of the buffer in bytes.
type#
uint8_t sl_wifi_buffer_t::type
Indicates the buffer type (SL_WIFI_TX_FRAME_BUFFER, SL_WIFI_RX_FRAME_BUFFER, and so on.) corresponding to the buffer.
data#
uint8_t sl_wifi_buffer_t::data[]
Stores the data (header + payload) to be send to NWP.