Use Case Scenario#
The current implementation of PTA is suitable for the following scenarios:
Low Wi-Fi usage and low throughput requirements
This use case allows occasional Wi-Fi disconnections. However, test results show no disconnections unless the frequency of REQUEST and PRIORITY signals increases significantly. All three PTA configurations are suitable for this scenario.
Moderate traffic on EFR32 devices with specific Wi-Fi throughput needs
When BT Classic, BLE, Zigbee, or Thread protocols are active on the EFR32 devices, and moderate Wi-Fi throughput is required, Configuration 3 is recommended.
Moderate traffic on both EFR32 (i.e., BT Classic/BLE, Zigbee, THREAD) and Wi-Fi.