Major Technical Specification of PTA#

The major technical specifications of PTA define key aspects that ensure efficient and reliable communication between Wi-Fi and Zigbee protocols. These specifications are summarized in the following table.

Sr No. Technical Parameter Description
1 Frequency Band Operates in the 2.4 GHz band
2 Protocols Supported Wi-Fi, Zigbee
3 PTA Configuration PTA Main: SiWG917 SoC
PTA Secondary: EFR32MG21 devices in Zigbee mode
4 Communication Interface Uses three GPIO connections for handshake signals and SPI for serial communication
5 Interference Management Protects Zigbee transmission/reception from Wi-Fi interference.
Includes provisions to protect Wi-Fi transmissions from Zigbee interference.
Future enhancements will address Wi-Fi reception protection.
6 PTA Schedules and prioritize packet transmission to minimize collisions.
Ensures fair access to the channel for both Wi-Fi and Zigbee devices.
7 Integration Implemented on the SiWG917 SoC, which integrates hardware and software components for efficient resource management and interference mitigation.